Explore the seamless integration of smart home devices using Renesas' DA16600 module, which incorporates a DA16200 Wi-Fi SoC and a DA14531 Bluetooth Low Energy SoC. In this demonstration, the DA16600 sensor module is showcased alongside Amazon Echo Dot and Google Nest Mini smart home hubs, connected via Wi-Fi 6 technology for enhanced capacity and connectivity. Utilizing Matter's Multi-hub feature, users can control smart lighting effortlessly, toggling between hubs with voice commands such as "Alexa, turn on the lights" and "Ok Google, dim the lights." Renesas' module promises not only quick and easy development but also unparalleled battery life, security features, and compatibility with a wide range of Matter-supported devices, from lighting and thermostats to media devices and beyond. Learn more at Renesas.com/matter.