RL78/G23-128p 快速原型开发板 (RL78/G23-128p FPB)
RL78/G23-128p 快速原型开发板配备有RL78/G23微控制器,是一款专用于各种应用原型开发的评估板。它具有与 E2 Lite 仿真器同等的内置仿真器电路,以便您编写/调试程序,而无需其他工具。标配Arduino Mega,Pmod™和Grove接口,具有高度的可扩展性,譬如能够访问微控制器的所有引脚...
[Upgrade to Version] Solution Toolkit QE for OTA V2.0.0: Development Assistance Tool for Cloud (PDF | English, 日本語)
・Support FreeRTOS v202210.01-LTS-rx-1.1.3(LTS #2), FreeRTOS v202210.01-LTS-rx-1.2.1(LTS #2)
・Support the Fleet Provisioning method
・Support RL78 Family RL78/G23 group
QE for OTA is a development assistance tool that enables easy trial of over-the-air (OTA) firmware updates with Amazon Web Services (AWS, Azure).
Product Name | Latest Ver. | Released | Taget Device (Note1) | Details | Download(Note2) | Operating Environment |
---|---|---|---|---|---|---|
QE for OTA | V2.0.0 | Mar 1, 2024 | RX Family RL78 Family | See Release Note | Download | Operating Environment |
Notes
RL78/G23-128p 快速原型开发板配备有RL78/G23微控制器,是一款专用于各种应用原型开发的评估板。它具有与 E2 Lite 仿真器同等的内置仿真器电路,以便您编写/调试程序,而无需其他工具。标配Arduino Mega,Pmod™和Grove接口,具有高度的可扩展性,譬如能够访问微控制器的所有引脚...
The CK-RX65N cloud kit enables users to securely connect to the cloud and explore the features of the Renesas RXv2 core based RX65N MCU Group and cloud services.
With...
The Renesas Starter Kit+ for RX65N-2MB is the perfect starter kit for developers who are new to the RX65N (Code Flash 2MB, Pin Count 176-pin). The kit includes an LCD...
The Renesas RX65N Cloud Kit is an RX65N microcontroller-based cloud communications evaluation kit which is an ideal evaluation environment for IoT device developers....
The Renesas Starter Kit+ for RX671 is the perfect starter kit for developers who are new to the RX671 (Code Flash 2MB, Pin Count 144-pin). The kit includes an LCD...
配备 32 位微机 RX 系列旗舰 RX72N,可使用 LCD 创建 GUI,还可进行语音输入/输出等 HMI 开发和 Wi-Fi/BLE、以太网等的物联网设备开发。 安装预装演示和仿真器电路后,您即可立即体验开发过程。
通过预装的固件更新功能,可将固件写入 microSD 卡进行更新。...
Renesas Starter Kit+ for RX72N is the perfect starter kit for getting started with RX72N (code flash 4MB, pin number 224-pin). LCD display module and on-chip debugging...
QE for OTA Tutorial: How to implement FreeRTOS OTA by using Microsoft Azure on RX65N
This tutorial walks you through setting up Microsoft Azure, creating initial firmware, and executing OTA with updated firmware using QE for OTA.
00:00 Opening
00:15 Preparing the demo project
04:10 Preparing initial firmware
06:15 Executing OTA
博客 | 2023年9月6日 | ||
博客 | 2023年4月19日 |
QE for OTA provides a graphical user interface that allows you to set up the cloud, import sample projects, manage IoT devices, create firmware, and start OTA updates.
The [OTA Manage IoT Device (QE)] view, which is used to manage IoT devices, has the following features.
Releases - renesas/iot-reference-rx - GitHub
202210.01-LTS-rx-1.1.3, 202210.01-LTS-rx-1.2.1
Releases - renesas/amazon-freertos - GitHub
202012.00-rx-1.0.0, 202012.00-rx-1.0.1, 202012.00-rx-1.0.2, 202107.00-rx-1.0.0, 202107.00-rx-1.0.1
Releases - renesas/azure-rtos - GitHub
6.2.1_rel-rx-1.0.0, 6.2.1_rel-rx-1.0.1
Releases - renesas/iot-reference-rl78 - GitHub
v202210.01-LTS-rl78-1.0.0
Board or Kit | OTA sample projects(including RTOS) |
---|---|
CK-RX65N (Recommended) | FreeRTOS v202107.00-rx-1.0.1, FreeRTOS v202210.01-LTS-rx-1.1.3(LTS #2), FreeRTOS v202210.01-LTS-rx-1.2.1 (LTS #2) |
AzureRTOS 6.2.1_rel-rx-1.0.1, AzureRTOS 6.2.1_rel-rx-1.0.0 | |
CK-RX65N v2 (Wi-Fi) (Recommended) | FreeRTOS v202210.01-LTS-rx-1.2.1 (LTS #2) |
RX65N-Cloud-Kit (Note1) | FreeRTOS v202107.00-rx-1.0.1, FreeRTOS v202107.00-rx-1.0.0 |
FreeRTOS v202012.00-rx-1.0.2, FreeRTOS v202012.00-rx-1.0.1, FreeRTOS v202012.00-rx-1.0.0 | |
RX65N-2MB-Starter-Kit-Plus (Note1) | FreeRTOS v202107.00-rx-1.0.1, FreeRTOS v202107.00-rx-1.0.0 |
FreeRTOS v202012.00-rx-1.0.2, FreeRTOS v202012.00-rx-1.0.1, FreeRTOS v202012.00-rx-1.0.0 | |
RX72N-ENVISION-KIT (Note1) | FreeRTOS v202012.00-rx-1.0.2 |
RX671-Starter-Kit-Plus (Note1) | FreeRTOS v202012.00-rx-1.0.2 |
RL78/G23-128p Fast Prototyping Board | FreeRTOS v202210.01-LTS-rl78-1.0.0 |
Note
1. Although the operation has been confirmed, it is recommended to use the CK-RX65N.