RXv3 Core has achieved 6.0 CoreMarks/MHz with CC-RX V3.04!
Renesas RXv3 Core performance has exceeded 6.0 CoreMarks/MHz of EEMBC’s CoreMark®. I will introduce this wonderful achievement and Renesas CC-RX compiler’s contribution to the higher score.
Renesas RXv3 Core performance has exceeded 6.0 CoreMarks/MHz of EEMBC’s CoreMark®. I will introduce this wonderful achievement and Renesas CC-RX compiler’s contribution to the higher score.
The RZ/A3UL microprocessor (MPU) reduces the number of required components contributing to lower total cost, including PCB development man-hours and software development costs.
With flexible development software and scalable options based on Arm Cortex-M33, M23 and M4 cores, the RA MCU family is becoming the top choice on which to base your IoT designs in industrial and building automation, metering, healthcare, and home appliances.
The operating voltage of high-end microcontrollers have recently been reduced to a lower voltage. However, the new RX660 will support 5V power systems, which are increasingly popular in the consumer electronics and industrial fields.
Renesas has variety of products that will help in developing an efficient and reliable pure sine wave inverter.
Functional safety has been in place for a long time and is wide and varied. Renesas Functional Safety solutions are IEC61508 certified to accelerate time to market and reduce total cost.
With the widely deployed cellular network in recent years, IoT devices can be easily implemented in any location. At the same time, battery-driven power supply is preferably adopted.
I will introduce the RX family solution that achieves low power consumption by combining the Cellular and FreeRTOS.
In order to collect meaningful data from the environment, sensors are now being used in many different applications. Using Sensor Fusion, real truth can be generated by combining multiple physical sensor data which would lead to reducing the uncertainty related to overall task performance. Through the application of deep learning for sensor fusion, intelligence and reliability among a wired range of industrial and consumer segments can be increased.
Since its release, RZ/V2M has been adopted by various Vision AI applications thanks to its ISP and dedicated AI accelerator (DRP-AI).
Target Board for RX Family is a series of entry-level boards of Renesas 32-bit RX MCU which provide users a fundamental and affordable hardware tool to start evaluating RX MCU or quickly build a prototype on it. In this blog, I am going to introduce the design of the Target Board and use a pre-prepared sample project to illustrate how to start working with a Target Board.