Enabling Good Air Quality in Our Homes with Next Generation Humidity Sensors
For the integration of devices like humidity and temperature sensors into our everyday lives and structures; performance, size, and power are critical factors.
For the integration of devices like humidity and temperature sensors into our everyday lives and structures; performance, size, and power are critical factors.
This blog presents the ZSSC3281, a fully innovative architecture for the next generation of sensor signal conditioners to support the design and performance features of smart sensors.
This blog introduces the software and tools for the RZ/V2M equipped ISP and DRP-AI, called AI accelerator. Users can start to develop vision AI products easily and immediately.
In this blog, the sample program for the FIR filter using the RX140 MCU will be introduced as an example of a DSP application that can be implemented at low cost.
Renesas is the only company offering a two-chip Wi-Fi 6/6E solution that supports Tri-Band Plus (concurrent transmission over 3 bands plus a dedicated listening radio) solution.
The new IoT development kits for both the RA and RX MCU families, support LTE CAT-M1 connectivity to simplify design and deployment to get new solutions to market faster.
This blog covers considerations helpful to those who are presently operating or deploying service with Wi-Fi 5 and are looking to move forward to Wi-Fi 6.
The RX66T 48-pin LFQFP 0.5mm-pitch optimized for single motor control in our RX-T series lineup is highly evaluated in the field of inverter control.
Artificial Intelligence coupled with real-time analytics provides businesses with exceptional insight into the consumer experience and IT workers are now prone to act rather than react to solve issues.
Small size, good performance and low power consumption…If you need a useful Arm® MCU, discover the advantages of RA2E2 32-bit microcontroller and its RA2E2 fast prototyping board.