Renesas SmartBond 4+
Renesas Electronics
Designed for iPad
-
- Free
Screenshots
Description
The SmartBond™ app from Renesas Electronics is a mobile application that works as a generic tool for interacting with Bluetooth® Low Energy devices.
With the app you can scan for and connect to Bluetooth® Low Energy peripherals. Multiple connections and scan filtering are supported. You can also use the app in peripheral mode, so that other devices can scan for and connect to it.
The app can act both as GATT client and GATT server. All GATT operations are supported. The app recognizes the Bluetooth® SIG adopted GATT objects, which are displayed with their proper names, their values are parsed and displayed as text, and, where supported, a custom write user interface is available. You can configure the GATT server and peripheral mode, either directly, or by cloning existing peripherals.
What’s New
Version 3.630.4
- Bug fixes and improvements.
App Privacy
The developer, Renesas Electronics, indicated that the app’s privacy practices may include handling of data as described below. For more information, see the developer’s privacy policy.
Data Not Collected
The developer does not collect any data from this app.
Privacy practices may vary, for example, based on the features you use or your age. Learn More
Information
- Seller
- Renesas Electronics Corporation
- Size
- 27 MB
- Category
- Utilities
- Compatibility
-
- iPhone
- Requires iOS 12.1 or later.
- iPad
- Requires iPadOS 12.1 or later.
- iPod touch
- Requires iOS 12.1 or later.
- Mac
- Requires macOS 11.0 or later and a Mac with Apple M1 chip or later.
- Apple Vision
- Requires visionOS 1.0 or later.
- Languages
-
English
- Age Rating
- 4+
- Copyright
- © 2022-2024 Renesas Electronics
- Price
- Free