Renesas SmartConsole 4+

Renesas Electronics

Designed for iPad

    • Free

Screenshots

Description

The SmartConsole app from Renesas Electronics is a mobile application that works with devices which support the Renesas CodeLess™ Service or the Dialog Serial Port Service (DSPS), such as Development Kits based on Renesas DA14585 and DA14531 Bluetooth® Low Energy SoCs.


With the app you can connect to CodeLess™ and DSPS devices. The app selects its initial user interface (UI) based on the supported services on the peer device. It supports command mode (CodeLess) and binary mode (DSPS) and can change between the two modes if both are supported by the peer device.


CodeLess™ allows control of the peer device, through a comprehensive set of AT commands. With these commands, you can read and modify settings on the peer device and control peripherals connected to it. You can issue AT text commands directly, through the AT console available in the app, or generate them from UI abstractions provided by the app.


The Dialog Serial Port Service (DSPS) from Renesas Electronics is a proprietary service over the Bluetooth® Low Energy protocol that emulates a serial cable communication. It provides a simple wireless substitute for wired (RS-232) connections.


With the app you can exchange data with other DSPS enabled devices. The functionality of the DSPS app is included in the SmartConsole app, so it can be used as a replacement of the DSPS app.

What’s New

Version 3.540.4

- Rebranded app UI from Dialog Semiconductor to Renesas Electronics

- DSPS: speed calculation, flow control indicators, file receive

- CodeLess security screen

- Bug fixes and improvements

App Privacy

The developer, Renesas Electronics, indicated that the app’s privacy practices may include handling of data as described below. For more information, see the developer’s privacy policy.

Data Not Collected

The developer does not collect any data from this app.

Privacy practices may vary, for example, based on the features you use or your age. Learn More

More By This Developer

See All
GATTBrowser
Utilities
Renesas SUOTA
Utilities
Renesas SmartTags
Utilities
Renesas SmartBond
Utilities
Renesas WiFiProvisioning
Utilities
Renesas SmartConfig
Utilities

You Might Also Like

See All
XT UART
Utilities
D230 Tool
Utilities
CrownSensor
Utilities
XTSpeed
Utilities
xBeaconPlus
Utilities
nRF Wi-Fi Provisioner
Utilities