Basic Library
Digital I/O
Analog I/O
Advanced I/O
Time
Math
Trigonometry
Random Numbers
Bits and Bytes
Interrupts
Serial Comm.
Standard Library
Servo Motor
Character LCD
SPI
I2C (Wire)
SD Card
SD (File Operations)
Periodic Operation
Clock (RTC)
Trigonometry
This library provides trigonometry functions, carrying out sin, cos and tan calculations.
sin
- Description
- Calculates the sine (sin) of an angle (in radians).
- Syntax
- sin(rad)
- Parameters
- rad: The angle in radians (float)
- Returns
- The sine of the angle (double)
cos
- Description
- Calculates the cosine (cos) of an angle (in radians).
- Syntax
- cos(rad)
- Parameters
- rad: The angle in radians (float)
- Returns
- The cosine of the angle (double)
tan
- Description
- Calculates the tangent (tan) of an angle (in radians).
- Syntax
- tan(rad)
- Parameters
- rad: The angle in radians (float)
- Returns
- The tangent of the angle (double)
Sample Program
#include <Arduino.h>
void setup(){
Serial.begin(9600);
}
void loop(){
// print labels
Serial.print("RAD"); // prints a label
Serial.print("\t"); // prints a tab
Serial.print("SIN");
Serial.print("\t");
Serial.print("COS");
Serial.print("\t");
Serial.print("TAN");
Serial.print("\t");
Serial.println("");
for(float x=0; x< PI; x+=0.01){ // only part of the ASCII chart, change to suit
// print it out in many formats:
Serial.print(x); // print as an ASCII-encoded decimal - same as "DEC"
Serial.print("\t"); // prints a tab
Serial.print(sin(x)); // print as an ASCII-encoded decimal
Serial.print("\t"); // prints a tab
Serial.print(cos(x)); // print as an ASCII-encoded hexadecimal
Serial.print("\t"); // prints a tab
Serial.print(tan(x)); // print as an ASCII-encoded octal
Serial.print("\t"); // prints a tab
Serial.println(""); // prints another carriage return
delay(100); // delay 100 milliseconds
}
}