Basic Library
Digital I/O
Analog I/O
Advanced I/O
Time
Math
Trigonometry
Random Numbers
Bits and Bytes
Interrupts
Serial Comm.
Standard Library
Servo Motor
Character LCD
SPI
I2C (Wire)
SD Card
SD (File Operations)
Periodic Operation
Clock (RTC)
I2C Communications (Wire)
This is an I2C communications library that facilitates two-wire class communications (also called "Wire Library"). The pull-up to communication lines is needed. There is a total of five channels available. You cannot use a slave device. The following information describes channels corresponding to pins, which can be confirmed by referring to the pin map.
To use, specify #include <Wire.h>.
Wire: 19(SCL), 18(SDA) (Software I2C)
Wire1: 1(SCL), 0(SDA)
Wire2: 6(SCL), 5(SDA)
Wire3: 8(SCL), 7(SDA)
Wire4: 11(SCL), 12(SDA)
begin
- Description
- Initiates the Wire library.
- Syntax
- Wire.begin(address)
- Parameters
- address: Specifies a 7-bit address when operating as a slave. It is not necessary during master operation.
- Returns
- None
requestFrom
- Description
- Used by the master to request bytes from a slave device. The bytes may then be retrieved with the available() and read() functions.
- Syntax
- Wire.requestFrom(address, quantity)
Wire.requestFrom(address, quantity, stop) - Parameters
- address: The 7-bit address of the device from which to request bytes.
quantity: The number of bytes to request.
stop: Boolean. True will send a stop message after the request, releasing the bus. False will continually send a restart after the request, keeping the connection active. - Returns
- Byte: The number of bytes returned from the slave device.
beginTransmission
- Description
- Begin a transmission to the I2C slave device with the given address. Subsequently, queue bytes for transmission with the write() function and transmit them by calling endTransmission().
- Syntax
- Wire.beginTransmission(address)
- Parameters
- address: The 7-bit address of the device to which to transmit
- Returns
- None
endTransmission
- Description
- Ends a transmission to a slave device that was begun by beginTransmission() and transmits the bytes that were queued by write().
- Syntax
- unsigned char Wire.endTransmission()
- Parameters
- None
- Returns
- 0: Success
1: Data too long to fit in transmit buffer
2: Received NACK on transmit of address
3: Received NACK on transmit of data
4: Other error
write
- Description
- Adds a character string or data to the end of the transmit buffer.
- Syntax
- Wire.write(value)
Wire.write(string)
Wire.write(data, length) - Parameters
- value: A value to send as a single byte
string: A string to send as a series of bytes
data: An array of data to send as bytes
length: The number of bytes to transmit - Returns
- Byte: Write() will return the number of bytes written, though reading that number is optional.
available
- Description
- Returns the number of bytes available for retrieval in the receive buffer.
- Syntax
- Wire.available()
- Parameters
- None
- Returns
- The number of bytes available for reading.
read
- Description
- Reads one byte of data from the receive buffer.
- Syntax
- Wire.read()
- Parameters
- None
- Returns
- The next byte received.
Sample Program
Receive 6 bytes of data from slave device at address 0x40.
#include <Arduino.h>
#include <Wire.h>
void setup()
{
Wire.begin(); // join i2c bus (address optional for master)
Serial.begin(9600); // start serial for output
}
void loop()
{
Wire.requestFrom(0x40, 6); // request 6 bytes from slave device #2
while(Wire.available()) // slave may send less than requested
{
char c = Wire.read(); // receive a byte as character
Serial.print(c); // print the character
}
delay(500);
}