ルネサス車載事業戦略の概要
このブログでは、ルネサスが自動車業界の進化をどのように捉え、事業戦略を描くか、ご紹介します。
このブログでは、ルネサスが自動車業界の進化をどのように捉え、事業戦略を描くか、ご紹介します。
How we can use the Data Operating Circuit and the Data Transfer Controller to create complete, autonomous subsystems that can make simple decisions based on measured data without CPU intervention.
Multiplexed Register Clock Driver (MRCD) and Multiplexed Data Buffer (MDB) components allow DDR5 memory modules to deliver significantly higher bandwidth for memory sub-systems in next-generation servers.
最新マイコンRX140が搭載するCTSU2SLの新機能を活用した自己容量耐水ソリューションにより、基板サイズの制約がある水回り用途でも静電容量式タッチキーを実現できます。
Renesas offers a solution that adapts well in remote locations where there is no Wi-Fi or Bluetooth LE access, only a cellular radio using CAT-M1; the inclusion of solar energy harvesting into the design allows for long-term battery life.
大規模化・複雑化するE/Eアーキテクチャの早期に開発に向けて、実機無しでデバイス間通信を伴うソフトウェア開発を可能とする、「マルチデバイス用協調シミュレーション環境」を提案します。
インダストリー4.0はプロセスの自動化に伴う大きな変革をもたらしており、 産業ネットワークを含むクラウドコンピューティングとエッジAI分析の統合は、次世代の産業オートメーションの再設計を担っています。
Introduces the concept of the Data Transfer Controller, a much more flexible and power method of transferring data between peripherals and memory compared to the traditional Direct Memory Access Controller.