ルネサスによる自動車機能安全サポート(3) –ISO 26262に適合したSEooCソフトウェア
本稿では、SEooC (Safety Element out of Context) ソフトウェア開発に関するISO 26262のガイダンスの大まかな概要を説明します。また、SEooCソフトウェア開発において一般的に発生する課題、およびルネサスのSEooCソフトウェアソリューションについても紹介します。
本稿では、SEooC (Safety Element out of Context) ソフトウェア開発に関するISO 26262のガイダンスの大まかな概要を説明します。また、SEooCソフトウェア開発において一般的に発生する課題、およびルネサスのSEooCソフトウェアソリューションについても紹介します。
The entry-level RA4E1 and RA6E1 MCUs address key design challenges including the optimal balance between performance and power consumption, as well as seamless migration options for future designs.
高精度AFE内蔵マイコンRX23E-Aと産業ネットワーク機能を強化したマイコンRX72Mを組み合わせることで、IoT時代にマッチしたデータアクイジション(DAQ)を実現することが可能です。
This blog gives a brief overview of CAN XL and 10MBit/s Ethernet, and the differences between them.
ルネサスが2020年後半にFSoEソリューションを発売して以来、このソリューションは世界中から注目されています。このブログでは、ルネサスのFSoEソリューションがどのように開発を容易にし、且つ開発期間を短縮するのかをご紹介します。
The Renesas RTD120D two-channel silicon-based thermopile can support healthy air in Canadian classrooms.
“ルネサスの戦略と幅広い車載ソリューションラインナップをアップデートさせていただく機会として「Renesas Automotive Daysオンライン」を開催します。
Wi-Fi 6, the next generation of wireless technology, offers higher speeds and improves signal reliability, network capacity and efficiency in dense deployments.
家電や産業機器の進化・IoT化に貢献してきたRX600シリーズに新製品RX671が加わりました。演算能力・機能が強化されたRX671の追加で、より幅広いニーズへの対応が可能となりました。
ルネサスはアプリケーション処理と標準的なEtherCAT通信、モータ制御をワンチップで実現するRX72M モータ+EtherCAT シングルチップソリューションをご提案します。