跳转到主要内容

概览

描述

This driver (sample program) uses the clock-synchronous serial I/O functions of a Renesas microcontroller to control reading, writing, and erasing of data.

特性

  • RX Family
    • Data can be read, written, and erased simply by calling user API functions.
    • Control is possible using the following serial interfaces of the microcontroller:
    • The clock-synchronous mode of the serial communication interface (SCI) and a single port are used for control.
    • Clock-synchronous operation (three-wire) of the serial peripheral interface (RSPI) and a single port are used for control.
    • The quad serial peripheral interface (QSPI) which is set to clock-synchronous operation and a single port are used for control.
  • RL78 Family
    • Data can be read, written, and erased simply by calling user API functions.
    • The SCI mode of the serial array unit (SAU) and a single port are used for control.
  • Learn More

目标设备

文档

设计和开发

样例程序

Additional Details

System Configuration

For systems on which the following devices are mounted, you can use it to control the each devices:

Slave DeviceSerial Flash Memory (SPI/QSPI), Serial Phase Change Memory (QSPI)
Master DeviceRenesas MCU (RX, RL78 Family)

Please refer to Supported Memory for detaild Memory Information, Target Devices and Product Lineup for detailed MCU information.

Support Memory

Renesas Electronics

Macronix International

Micron Technology

  • M25P Series SPI Serial Flash memory (SPI)
  • M45PE Series SPI Serial Flash memory (SPI)
  • P5Q Serial Phase Change Memory (SPI/QSPI)
  • N25Q Serial NOR Flash memory (SPI/QSPI)

Target Devices and Product Lineup

Here we present each software lineup by MCU. Please refer to each application note for a corresponding Integrated Development Environment.

 RX Family (FIT module)  RL78 Family (SIS module)  Other

RX Family (FIT module)

The software components shown in the figure below are FIT modules based on the Renesas Firmware Integration Technology (FIT). You can easily embed sample code in user applications by combining the required FIT modules. For example, you can use the DMAC or DTC FIT module to handle transfer by the DMAC or DTC. (About FIT)

图像
RX Family FIT Block Diagram
Sample Program list
Slave Device Control Software (Higher-level layer of the software)
Target MemoryApplication Note Title
MX25/66L family serial NOR flash memory
MX25R family serial NOR flash memory
(by Macronix International)
RX Family Clock Synchronous Control Module for Serial NOR Flash Memory Access Firmware Integration Technology Rev.3.51 - Sample Code (ZIP)
Clock Synchronous Single Master Control Software (Lower-level layer of the software)

RL78 Family (SIS module)

The RL78 family serial NOR flash memory control modules shown in the figure below are SIS modules based on the Software Integration System (SIS) approach. You can easily embed sample code in user applications by using such SIS modules with the Code Generator included in the Smart Configurator. For example, you can use the Code Generator to produce code for handling transfer by the RL78 family data transfer controller.

图像
RL78 Family SIS Block Diagram

* Refer to the application note RL78 Family Serial NOR Flash Memory Control Module Software Integration System.

Target MemoryApplication Note Title
AT25QF SPI FlashRenesas ElectronicsRL78 Family Serial NOR Flash Memory Control Module Software Integration System Rev.1.00 - Sample Code (ZIP)
QT25SF SPI Flash
MX25/66L family serial NOR flash memoryMacronix International
MX25R family serial NOR flash memory

Other

Sample Program list

RX (except FIT module), RL78(except SIS module)Family

图像
Block Diagram
Slave Device Control Software (Higher-level layer of the software)
Clock Synchronous Single Master Control Software (Lower-level layer of the software)

R8C and M16C Family

The following software controls the slave device and master device in systems that include M16C or R8C Family MCUs.

Slave Device and Master Device Control Software (Common Software)
Target MCUApplication Note Title
R8C and M16C FamilySerial Flash Driver Sample Program (ZIP)