2024-06-14

Sixth in the RX security video series – Renesas walks through the process of encrypting the application program and performing a Secure Firmware Update using the Renesas Secure Flash Programmer so that the plain text of the application program to be updated is not exposed when updating the application program.

Chapter's Title

0:00:00 Opening
0:00:23 Recommended Viewing
0:00:53 Secure Factory Programming
0:02:16 Secure Firmware Update
0:07:50 For more information