画像
![boards-kits](/sites/default/files/styles/banner_424x349/public/media/images/design-support_boards-kits-2016x349.jpg?itok=wDqOIL--)
ルネサスマイコン評価のためのユーザフレンドリーな開発環境をご提供します。
製品番号 | タイトル | 分類 | 会社名 |
---|---|---|---|
5P49V6965-PROG | Programming Kit for VersaClock® 6E | Development | Renesas |
89KTPEB383-QFN | System Development Kit for the PEB383 PCIe to PCI Bridge | Development | Renesas |
89KTPEB383-QFP | System Development Kit for the PEB383 PCIe to PCI Bridge | Development | Renesas |
89KTPES12N3 | System Development Kit for the PES12N3 PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES12N3A | System Development Kit for the PES12N3A PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES16H16 | System Development Kit for the 89HPES16H16 PCI Express System Interconnect Switch | Development | Renesas |
89KTPES16T4 | System Development Kit for the PES16T4 PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES16T4A | System Development Kit for the PES16T4A PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES16T7 | System Development Kit for the PES16T7 PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES22H16 | System Development Kit for the 89HPES22H16 | Development | Renesas |
89KTPES22H16G2 | System Development Kit for the 89H22H16G2 | Development | Renesas |
89KTPES24N3 | System Development Kit for the PES24N3 PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES24N3A | System Development Kit for the PES24N3A PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES24NT3 | System Development Kit for the 89HPES24NT3 | Development | Renesas |
89KTPES24T3 | System Development Kit for the 89HPES24T3 | Development | Renesas |
89KTPES24T6 | System Development Kit for the PES24T6 PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES32H8 | System Development Kit for the PES32H8 PCI Express System Interconnect Switch | Development | Renesas |
89KTPES32T8 | System Development Kit for the PES32T8 PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES34H16G2 | System Development Kit for the 89H34H16G2 | Development | Renesas |
89KTPES48H12 | System Development Kit for the PES48H12 PCI Express System Interconnect Switch | Development | Renesas |
89KTPES48H12AG2 | System Development Kit for the 89H48H12AG2 | Development | Renesas |
89KTPES48T12 | System Development Kit for the PES48T12 PCI Express I/O Connectivity Switch | Development | Renesas |
89KTPES4T4G2 | System Development Kit for the 89HPES4T4G2 | Development | Renesas |
89KTPES64H16 | System Development Kit for the PES64H16 PCI Express System Interconnect Switch | Development | Renesas |
89KTPES64H16AG2 | System Development Kit for the 89H64H16AG2 | Development | Renesas |
89KTPES64H16G2 | System Development Kit for the 89H64H16G2 | Development | Renesas |
89KTPES6T5 | System Development Kit for the 89HPES6T5 | Development | Renesas |
89KTPES8NT2 | System Development Kit for the 89HPES8NT2 | Development | Renesas |
89KTPES8T5 | System Development Kit for the PES8T5 PCI Express I/O Expansion Switch | Development | Renesas |
89KTPES8T5A | System Development Kit for the 89HES8T5A | Development | Renesas |
AB2-AML100 | Aspinity AB2 AML100 Application Board | Development | Aspinity, Inc. |
ASI-PROG-KIT | ASI Programmer Kit USB | Development | Renesas |
AVSHORIZONE | Avnet Silica HoriZone RA Powered by Renesas | Development | Avnet |
BDE-BLEM301 | Bluetooth® 5.1 Low Energy Module | Development | BDE Technology Inc. |
BLUETOOTH-LE-TINY-CLICK | Mikroe Bluetooth® LE TINY Click™ with SmartBond™ DA14531 Module | Development | MikroElektronika |
CK-RA6M5 | RA6M5 MCUグループをベースにしたクラウドキット | Development | Renesas |
CK-RX65N | RX65N MCUグループによるクラウドキット | Development | Renesas |
DA14530-00FXDB-P | SmartBond TINY™ DA14530 Bluetooth® Low Energy Dev Kit Pro - FCGQFN24 Daughterboard | Development | Renesas |
DA14530-00FXDEVKT-P | SmartBond TINY™ DA14530 Bluetooth® Low Energy 5.1 System-on-Chip Development Kit Pro | Development | Renesas |
DA14531-00FXDB-P | SmartBond TINY™ DA14531 Bluetooth® Low Energy 5.1 System-on-Chip Development Kit Pro - FCGQFN24 Daughterboard | Development | Renesas |
DA14531-00FXDEVKT-P | SmartBond TINY™ DA14531 Bluetooth® Low Energy 5.1 System-on-Chip Development Kit Pro | Development | Renesas |
DA14531-00FXDEVKT-U | SmartBond TINY™ DA14531 Bluetooth® Low Energy 5.1 System-on-Chip USB Development Kit | Development | Renesas |
DA14531-00OGDB-P | SmartBond TINY™ DA14531 Bluetooth® Low Energy 5.1 System-on-Chip Development Kit Pro - WL-CSP Daughterboard | Development | Renesas |
DA14531-01FXDB-P | SmartBond TINY™ DA14531-01 Bluetooth® Low Energy Dev Kit Pro - FCGQFN24 Daughterboard | Development | Renesas |
DA14531MOD-00DEVKT-P | SmartBond TINY™ DA14531 Bluetooth® Low Energy 5.1 システムオンチップモジュール開発キットPro | Development | Renesas |
DA14531MOD-00F1DB-P | SmartBond TINY™ DA14531 Bluetooth® Low Energy 5.1 System-on-Chip Module Development Kit Pro - Daughterboard | Development | Renesas |
DA14535-00FXDB-P | SmartBond™ DA14535 Bluetooth® Low Energy 5.3 SoC開発キットProドータボード | Development | Renesas |
DA14535-00FXDEVKT-P | SmartBond TINY™ DA14535 Bluetooth® Low Energy 5.3 SoC開発キットPro | Development | Renesas |
DA14535-00FXDEVKT-U | SmartBond TINY™ DA14535 Bluetooth® Low Energy 5.3 SoC USB開発キット | Development | Renesas |
DA14580-DONGLE | DA14580 Bluetooth® Low Energy USB Dongle | Development | Renesas |