Skip to main content
Renesas Electronics Corporation

Overview

Description

FreeRTOSTM software platform for RX MCUs: helping to reduce system development times

Renesas FreeRTOS makes it easy to create applications using FreeRTOSTM with Firmware Integration Technology (FIT) and Smart Configurator.
For details, refer to the wiki page on Github.

Features

  • You can use the open-source FreeRTOSTM real-time OS in developing multi-tasking applications.
  • Take advantage of the hardware by combining the middleware and device drivers we provide with the real-time OS.
  • This package allows you to start using the peripheral functions of RX MCUs at once, and can shorten times taken in considering prototypes.
  • Applications which utilize FIT can be used for all RX-series products, and can reduce the cost of developing software as you expand your product development.

Target Devices

Note: For the latest information on target devices, refer to Supported device on the wiki page on Github.

Documentation

Support

Support Communities

  1. FreeRTOS on RX63N

    ... project using e2studio, RX63N microcontroller, GCC compiler and FreeRTOS. I downloaded the FreeRTOS archive, but there is no RX63N demo project in it. I added FreeRTOS to my RX63N e2studio project manually, but it does not work. I can not be sure that I added FreeRTOS correctly. For example, I ...

    Sep 15, 2021
  2. R5F524UEAxFB and FreeRTOS_RX_v10.0.04

    why e2studio 7.8.0 cannot allow to create a project for R5F524UEADFB using FreeRTOS_RX_v10.0.04 stating device not supported? Thanks F

    Feb 18, 2022
  3. FreeRTOS for RX Family

    I'm currently trying to get a FreeRTOS project started for the RX231. The only sample code I have been able to find is 5 years old. That is too old. When I search "FreeRTOS sample code" on Renesas' site, the search doesn't even turn that up. It finds ...

    Feb 20, 2020
View All Results from Support Communities (22)

Knowledge Base

  1. Changing data endian setting of a RX project

    ... mbig-endian-data setting does not affect to bitfield order. You should re-order bitfields when migrating source files from little endian projects. Note for FreeRTOS projects:In FreeRTOS projects, several descriptions should be changed such as follows. File and line location of description may be different among FreeRTOS versions ...

    Mar 4, 2022
  2. RX Family: How to update the firmware

    ... memory via USB (Mass Storage Class).[RX Family Internal Flash ROM rewrite program via USB Mass Storage (R01AN3503)][sample code (R01AN3503)] Firmware is updated by FreeRTOS OTA using Amazon Web Services. The e2 studio allows you to download sample projects from GitHub.[RX Family How to implement FreeRTOS OTA using ...

    Jun 3, 2026
  3. Creating FreeRTOS (with IoT libraries) projects in e² studio

    For RX Family, LTS packaging of FreeRTOS with IoT libraries is available. The board CK-RX65N-V2 is supported. The LTS 202406 is available in e² studio 2025-01 or later. Please see this page for more information on the package. https://github.com/renesas/iot ...

    Mar 19, 2025
View All Results from Knowledge Base (6)