Overview
Description
This assembler package includes the SRA74 assembler. The powerful optimizations offer the ultimate in execution speed and code efficiency, and the utilities increase productivity.
Features
- Structured instructions
- Versatile macro instructions
- Automatically selects memory-efficient addressing modes
- Tag files generation
- Library function
- Free software including an absolute address list generation tool, multiple file cross referencer and others
- Learn More
Release Information
Latest Ver.: V.4.10 Release 02
Released: Oct 1, 2005
Details of upgrade (See Tool News)
Standard life cycle of Compilers (PDF | English, 日本語)
Note: Future functional extension or problem fixes are not planned.
Target Devices
Additional Details
Functions (SRA74 Assembler)
- Structured instructions
- Supports C language-like assignment statements and control statements (e.g. if, for). These structured instructions clarify program's control structure and improve productivity and maintainability.
- Bit symbol: By using structured instructions, a memory bit and accumulator bit can be referenced and modified.
Example of modifying accumulator bit in a assignment statement: BIT_A0 = 0 Example of referencing a accumulator bit in a IF statement: if BIT_A0
The memory bit is defined as a bit symbol. The accumulator bit has reserved words. - Accessing directly to the internal register: By using structured instructions, the internal register and flag can be referenced and modified.
Example of modifying the internal register in a assignment statement: C = 1 Example of referencing the internal register in a IF statement: if C == 0
The internal register and flag have reserved words.
- Bit symbol: By using structured instructions, a memory bit and accumulator bit can be referenced and modified.
- Versatile macro instructions
- Frequent instructions are defined as macro instructions to clarify programs. SRA74 supports system macro instructions and user-definable macro instructions.
- Tag files generation
- SRA74 generates tag files storing assembling error information. With the tag files, source files can be efficiently modified.
- Library function
- LIB74 librarian generates a library of versatile subroutines, which improves the diversion rate of programs.
- Absolute address lists
- LST74 generates an absolute address list file from relative address list files to aid in understanding overall program organization.
- Cross reference lists
- SRA74 generates 2 kinds of cross-referencers which generate lists of definitions and references of labels and symbols. One cross-referencer is CRF74 which generates cross reference lists in each source file, and the other is XREF74 which generates a cross reference list in more than two source files. These lists help check dependencies of labels and symbols during debugging.
- Branch instruction optimizing
- The LOOP74 converts from a branch instruction which causes the assembler error because of the branch address outside the legal range to the instruction that can branch without problems. With LOOP74, you can create a program including best branch instructions from one using shortest branch instructions.
Product Components
- Relocatable assembler: sra74
- Linker: link74
- Librarian: lib74
- Cross referencer: crf74
- File converter for M37280: cv74
- Branch optimization tool: loop74
- Machine language file converter: hextos2
- Multiplication & division sub-routine: sra74.a74
- Absolute address list generation tool: lst74 (Note1)
- Cross referencer for multiple files: xref74 (Note1)
- PDF manual
- Help file
- Simulator debugger: Provides source level debugging capability in targetless system-level.
- IDE (Integrated development environment): High-performance Embedded Workshop and TM: Provides seamless integration and easy access to all tools for coding, compiling, linking, and debugging. It greatly increases productivity.
Note
- These are free software, therefore the provisions of the license are not applied.
Processing Flow
Support
Support Communities
Get quick technical support online from Renesas Engineering Community technical staff.
Knowledge Base
Browse our knowledge base for helpful articles, FAQs, and other useful resources.