Skip to main content
Renesas Electronics Corporation

Restrictions : Windows® 7

Restrictions on development tools under Windows® 7 are described below

No.1 Restriction on starting device file installer (DFINST V3.30 or later)

[Description]Device file installer may not start from PM+.
[Workaround]Run device file installer from Windows start menu.

No.2 Restriction on registering device file (DFINST V3.30 or later)

[Description]Device file is not registered to registry by dragging and dropping device file on device file installer.
[Workaround]Use button on device file installer to register device file.

No.3 LDG does not support Windows® 7

[Description]LDG has not been supported Windows® 7.

No.4 Restriction on not displaying the registered external tool's icon on PM+

[Description]If the external tool bar is displayed soon after registering one external tool without the registered external tools, the icons of the registered external tools are not displayed.
[Workaround]Restart PM+.

No.5 Restriction on display in Register window

[Description]In case of selecting [Hide All] in Register Select dialog with expanding register (ex. [+PSW]) in Register window, unnecessary data will be remained on this window.

No.6 Not support dual core PC

[Description]Personal computers that incorporate dual/multi-CPUs or the Hyper-Threading function are not supported.