Skip to main content

How to Debug FreeRTOS Using Tracealyzer for RX

How to Debug FreeRTOS Using Tracealyzer for RX
Sep 15, 2023

This video explains the preparation to launch Tracealyzer® during application development in e2 studio for the Renesas RX Family.
See also the application note Tracealyzer® for FreeRTOS Debugging Rev1.01 (PDF | English, 日本語)

00:00 Opening
00:24 Preparing to debug FreeRTOS with Tracealyzer®
01:19 Creating a project to operate Tracealyzer® via UART
05:51 Connecting the host PC and CK-RX65N board
06:37 Starting debugging of a project with Tracealyzer®