Jun 27, 2023
About This Video
This video uses the RX72N as an example to explain the settings for copying the flash memory reprogramming code to RAM using the flash module FIT.
Application note: RX Family Flash Module Using Firmware Integration Technology Rev.5.22
(PDF | English, 日本語)
00:00 Opening
00:29 About reprogramming process that needs to be copied to RAM
01:00 Part 1: Settings when using CC-RX compiler
03:18 Part 2: Settings when using GCC compiler
03:56 Part 3: Settings when using IAR systems compiler