Skip to main content

IDT Introduces High-speed Multiplexer for DDR4 NVDIMM Technology; Selected by Micron as Preferred Supplier

New High-Speed Multiplexer is Designed for the Enterprise and Cloud Server Markets

October 10, 2015

SAN JOSE, Calif., Feb. 24, 2015-- Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today introduced a high-speed multiplexer that expands the company’s existing portfolio of DDR4 products targeting the nascent NVDIMM (non-volatile dual in-line memory module) ecosystem. Additionally, Micron Technology has selected IDT as its preferred supplier for NVDIMM multiplexers, which target the enterprise and cloud server markets.

NVDIMM is a new architecture that provides data persistence to DRAM (dynamic random-access memory) by allowing data to be backed up to non-volatile memory, such as flash memory, during special events including catastrophic power failure. Multiplexers are key components of NVDIMM architecture, isolating the host controller from the DRAM memory during "save" and "restore" operations between DRAM and non-volatile memory.

Multiplexers have traditionally placed a burden on the signal integrity of the memory channel, which can compromise the speed of the operation. IDT's high-speed multiplexer is designed to mitigate the signal integrity impact to the memory channel while enabling DDR4 NVDIMM applications to run at bus rates of up to 2133 MT/s (megatransfers per second)  and beyond.

“Micron is committed to significantly improving the performance of applications and systems by leveraging persistent memory,” said Robert Feurle, Micron vice president, Compute & Networking Marketing. “Our team has worked closely with IDT to develop a new high-speed multiplexer. This new multiplexer will be used on Micron DDR4 NVDIMM products.” 

The 12-bit bus switch/multiplexer comes in a VFBGA 48-pin package, for a compact footprint that can replace data buffers on the DIMM for NVDIMM applications. It features a make-before-break circuit that prevents glitches when switching, and AC and DC parameters optimized for DDR4, enabling the highest possible memory channel performance for NVDIMMs even when intermixed with other DIMM types.

“The potential of persistent main memory in server and storage systems is in the very early innings of being realized,” said Rami Sethi, vice president and general manager of IDT’s Memory Interface Products. “As a leading component supplier for DDR4 NVDIMMs, including  NVDIMM registered clock drivers (RCD), temperature sensors  and now multiplexers, we have diligently worked with leading companies like Micron to develop solutions that deliver best-in-class performance in both homogeneous and heterogeneous memory channel populations.”

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. Micron (Nasdaq:MU) is a trademark of Micron Technology. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on