Realize Real-Time Processing and Pre-warning of Information Covering 360 Degree Around the Vehicle and Contribute to Faster Time-to-Market of Safe and Secure Driving Support Systems

October 6, 2016

TOKYO, Japan, October 6, 2016 - Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the global availability of its expansive lineup of V2X solutions that will help accelerate the arrival of autonomous driving. The solutions include two system-on-chips (SoCs) that will ease the development process for vehicle-to-vehicle (V2V) and vehicle-to-infrastructure (V2I) communication systems. One of the solutions includes the R-Car W1R 760 megahertz (MHz) band wireless SoC for the Japanese market, and the new R-Car W2H SoC that features a high-performance security engine that is indispensable for V2X systems designed for the Japanese, U.S., and European markets. The other solution consists of the W2H SoC combined with the R-Car W2R 5.9 GHz band wireless communication SoC developed for U.S. and European markets.

By combining these new SoCs, system developers can now easily develop systems that support the corresponding V2X standard for the Japanese, U.S., and European markets. Renesas also delivers development starter kits that will enable system developers to immediately start application software development, leading to significant reductions in the development period for V2X systems.

In October 2015, Renesas launched the R-Car W1R, which conforms to Japan's wireless communications standards, and is adopted in the ITS Connect (Note 1) V2V and V2I communications system. It is the only device in the world with a proven track record that is currently commercially deployed in the V2X wireless SoC market. The R-Car W1R was adopted in Denso Corporation's in-vehicle ITS units. These units are also used in Toyota's Crown, Prius, and Lexus RX models for displaying traffic signal violation, cross traffic, and pedestrian warnings at traffic signals using car and infrastructure communications to warn drivers about approaching emergency vehicles and to assist cruise control and other functions.

In addition to the current V2X activities led by Japan, steady progress is being made in U.S. and European investment plans due to legislation and implementation of V2X technology. At the same time, the countries’ differing communication frequencies, communication standards, and security standards have made optimizing devices for each region and the associated software development into significant challenges for V2X system development. To ease these burdens, Renesas delivers V2X kit solutions that combine either the R-Car W1R or R-Car W2R with the R-Car W2H. These kit solutions make it possible to construct optimal systems for each region at low cost.

Key features of the V2X solutions:

(1) Kit solutions conform to Japanese, U.S., and European standards to support user system development

Systems that conform to the ARIB STD-T109 Japanese wireless communications standard as well as the ITS Connect security and communications standards can be implemented by combining the R-Car W1R, which is designed for the Japanese market, with the R-Car W2H. Similarly, systems that conform to the North American standards (IEEE 801.11p, IEEE 1609.x, and others) or the European ETSI standards, can be implemented by combining the R-Car W2R, which is designed for the European and U.S. markets, with the R-Car W2H.

Lineup of Renesas wireless communications SoC kit solutions:

  • R-Car W1R: Wireless communications SoC that supports the Japanese communications standards (760 MHz band).
  • R-Car W2R: Wireless communications SoC that supports the European and US communications standards (5.9 GHz band)
  • R-Car W2H: V2X communications processor SoC that supports the Japanese, US, and European security standards.
  • R-Car W1R + R-Car W2H kit: Implements V2V and V2I communication systems for the Japanese market.
  • R-Car W2R + R-Car W2H kit: Implements V2V and V2I communication systems for the European and US markets.

(2) V2X starter kits support rapid development and faster time-to-market

Renesas provides starter kits that support the Japanese, U.S., and European standards, and provides basic software packages (BSP: products that include operating systems, drivers, firmware, and middleware) for V2X communication processors, which will simplify user development of application software. To lower barriers to entry to the market, Renesas also provides wireless communication evaluation tools. These tools support a wide range of evaluation and testing for the system developer’s complex wireless communication characteristics evaluations, from the system development prototyping stage to wireless communication tests in the mass production stage to in-vehicle testing at the OEM manufacturer's site.

V2X starter kits that support Japanese, US, and European markets:

  • For the European market: RTK00V2XRC7746SBS
  • For the North American market: RTK00V2XRC7746SCS
  • For the Japanese market: RTK00V2XRC7746SDS

Availability

Samples of the R-Car W1R and R-Car W2H are available now. Mass production of the R-Car W2H is scheduled to begin in October 2017 and is expected to reach a volume of 300,000 units per month by 2019. (Availability is subject to change without notice.)

Renesas will demonstrate the new V2V and V2I solutions at the ITS World Congress 2016, October 10 to 14, 2016, in Melbourne, Australia.

Please refer to the separate sheet (PDF: 114 KB) for the main specifications of the R-Car W1R and R-Car W2H.

For more information on the V2X Communication, please visit: https://www.renesas.com/en/solutions/automotive/adas.html

For more information on the R-Car W1R, please visit:https://www.renesas.com/en/solutions/automotive/soc/r-car-w1r.html

For more information on the R-Car W2H, please visit: https://www.renesas.com/en/solutions/automotive/soc/r-car-w2h.html

(Note 1) ITS Connect: This is the general term for driving assistance systems that use the ITS dedicated frequencies stipulated by the ITS Connect Promotion Consortium. For more information, please visit: https://www.itsconnect-pc.org/en/

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on