Skip to main content
Renesas Electronics Corporation

IDT Extends 1.8 V RF Timing Family with Dual-Channel Buffer Devices that Deliver High Performance, Low Power

The 4 New Dual-Channel Members of the 8P34S LVDS Buffer Family Enable Fanout of High-frequency Clock and Data Signals with Very Low Additive Phase Jitter

November 28, 2016

SAN JOSE, Calif., Nov. 28, 2016— Integrated Device Technology, Inc. (IDT) (NASDAQ: IDTI) today introduced four high-performance, low-power, LVDS dual-channel fanout buffers, delivering high performance and power savings for system and board designers. Ideal for wireless infrastructure and other communications equipment, the new 1.8 V members of the IDT® 8P34S buffer family enable the simultaneous fanout of high-frequency clock and data signals, with very low additive phase jitter of typically  <45 femtoseconds.

Each of the devices’ two independent buffer channels offers up to eight low-skew outputs. Effective isolation between channels minimizes noise coupling. AC characteristics such as propagation delay are matched between channels.

Delivering up to 50 percent lower power than comparable competitive devices, IDT’s  dual-channel buffers allow board designers to reduce power consumption while maintaining clock performance. The buffers also enable engineers to move to lower supply rails in support of deeper submicron silicon processes.    

 “Relative to system timing distribution, RF designers no longer have to make power consumption trade-offs at the benefit of optimizing signal to noise ratio,” said Kris Rausch, general manager, timing products, at IDT. “These new devices offer superb AC characteristics at a low 1.8 V power supply; a combination that assists designers in maintaining optimum signal-to-noise performance as well as lower power consumption and less heat dissipation.”

The new devices enable two different signals to be buffered while remaining synchronous with one another; one channel can be used for a clock, the other for a synchronization signal or data, as applicable in device clock and SYSREF signal distribution in JESD204B applications. The power reduction allows higher system packing densities, saves cost in the power supply and cooling, and delivers lower power footprints.

The buffers’ low additive phase jitter, high spurious attenuation and low clock output skew are combined with high clock frequency support. Their compatibility with LVDS devices make them easy to use, and they are compatible in pin and function to equivalent industry standard 2.5 V and 3.3 V parts from IDT.

The latest members of the 8P34S buffer family join five previously introduced single-channel members.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, timing, wireless power transfer, serial switching, interfaces, automotive ASICs, battery management ICs, sensor signal conditioner ICs and environmental sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT can be found at www.IDT.com. Follow IDT on FacebookLinkedInTwitter, YouTube and Google+.

###

© 2016, IDT. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. or its wholly-owned subsidiaries around the world. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective