TOKYO, Japan, August 30, 2011 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the availability of its new SuperSpeed Universal Serial Bus (USB 3.0) SATA3 bridge system-on-chip ([SoC], part number, µPD720230) that enables data transfer between a USB3.0 host system and a Serial ATA (SATA) device in external USB storage equipment. The new SoC is the world's first USB 3.0 Bridge SoC that supports the UASP (USB Attached SCSI Protocol) protocol that significantly speeds up data throughput for large volumes of data.
USB 3.0 achieves data transfer speeds more than 10 times faster than the previous version of the standard, USB 2.0 (currently the mainstream data transfer technology) and therefore easily supports the growing need for increased data-recording media capacities. Renesas has led the industry by releasing the µPD720200 USB 3.0 host controller in May 2009 and began mass production in June that same year. Since then, the company's lineup of USB 3.0 host controllers has been widely adopted by customers worldwide. Total shipments of these products have already exceeded 40 million units since May 2010, and Renesas has ramped up production of its USB 3.0 host controllers to 6 million units per month. During this period, the company also released in December 2009 a UASP driver that achieves high-speed data transfers for storage devices by improving the performance limit of the BOT (Bulk-Only Transfer) standard used by USB 2.0, making it possible for external storage devices to take advantage of the increased speed offered by the new USB 3.0 standard.
Now, to respond to the need for even faster data transfer performance necessary with the increased scale of the data handled in the storage device market, Renesas has released the µPD720230 bridge SoC. This device, combined with Renesas' advanced host-controller technology and UASP driver software, achieves industry-leading data transfer performance.
In addition to Renesas USB 3.0 host controllers, the UASP driver operates with AMD's A70M and A75 chipsets, which has been made possible through close cooperation with AMD. Renesas also plans on achieving compatibility with AMD's future USB3-supporting chipsets.
Key features of the new µPD720230 SoC:
(1) Support for SATA Revision 3.0 enables 6 Gbps high-speed data transfer
The µPD720230 USB 3.0-SATA3 bridge SoC supports SuperSpeed USB transfer speeds of up to 5 gigabits per second (Gbps)—as well as the SATA Revision 3.0 6Gbps bit rate achieving maximum data transfer performance of USB 3.0.
(2) Supports both the UASP and BOT protocols and achieves data transfer performance that exceeds 370 megabytes per second (MB/s) in UASP mode
In addition to the BOT standard for mass storage devices using USB 2.0, it also supports the UASP protocol standardized in USB 3.0 for improving the performance limits of the BOT standard. When connected to an SSD that supports 6 Gbps SATA3, the µPD720230 device achieves data transfer performance in excess of 370 MB/s in UASP mode as verified by the ATTO Disk Benchmark, version 2.46.
(3) Realizes miniaturization and reduced power consumption of the end products
The µPD720230 USB 3.0 SATA3 SoC is provided in a 48-pin QFN package, incorporates a voltage regulator, and also supports bus power modes, which contribute to miniaturization of the end products.
Although only two states, the U0 normal state and the U3 suspend state were stipulated in the USB 2.0 standard, the USB 3.0 standard also stipulates the U1 and U2 power states to provide even finer-grained suppression of power consumption. The new USB 3.0 SATA3 SoC reduces overall power consumption by approximately 40 percent (when the system is in the idle state) via the new USB 3.0 U1 and U2 power states, as compared to when stipulating only the U0 and U3 power states.
Additionally, the USB 3.0 is capable of supporting data transfer rates of up to 5 gigabits per second (Gbps), which is 10 times faster than the previous USB 2.0 transfer speeds. Therefore, the USB 3.0 can reduce the data transferring time to 10 percent from that of the USB 2.0 and automatically extends the idle time. As a result, by stipulating the U1 and U2 power states, the new SoC realizes even more power conservation effect.
(4) The Renesas UASP driver is tested to ensure compatibility with Renesas' USB 3.0 host controllers and AMD's PC motherboard integration of the USB 3.0 interface.
Renesas' UASP driver runs not only on the Renesas µPD720200 USB 3.0 host controller and its follow-on products, the µPD720200A, µPD720201 and µPD720202, but also on AMD's A70M and A75 chipsets based on a cooperative agreement with AMD, as well as others. In addition, Renesas also plans on achieving compatibility with future AMD USB3-supporting chipsets with this driver.
(5) Renesas UASP driver is available for license to companies making USB 3.0 to SATA3 bridge devices
A license of Renesas' UASP driver is included with the company's µPD720230 USB 3.0 to SATA3 Bridge and is available for license to other SATA bridge manufacturers. Renesas has already concluded a licensing agreement with Japanese LSI supplier Media Logic.
“Through AMD's collaboration with Renesas, we were first in industry to offer integrated UASP via our USB3-enabled chipsets supporting our A-Series APU platforms,” said Godfrey Cheng, Director of the Client Technology Unit at AMD. “AMD customers will enjoy fully-validated support for Renesas µPD720230 USB 3.0 SATA3 SOC supporting UASP technology.”
More information for the specifications of the µPD720230 USB 3.0 SATA3 SoC can be found on the separate sheet.
Availability
Samples of Renesas Electronics' µPD720230 device are available now, priced at $3.5 per unit. Mass production is scheduled to begin in October 2011 with a combined production volume of 500,000 units per month expected. (Pricing and availability are subject to change without notice.)
Leadership in USB
As a member of the USB Implementers Forum (USB-IF) since 1996, Renesas Electronics (formerly NEC Electronics) has played a leading role both in defining USB standards and in developing USB technology. In April 2000, the company (then NEC Electronics) launched the µPD720100 device, the world's first USB 2.0-compliant host controller chip and an extensive lineup of other USB devices, and has earned a reputation for delivering dedicated customer service and high quality.
In May 2009, Renesas Electronics (then NEC Electronics) introduced the industry's first USB 3.0 xHCI host controller and, only after four months of its release, the company became the world's first to earn the “Certified SuperSpeed USB (USB 3.0)” certification from the USB-IF, and also started mass production of the µPD720200 host controller. In the following year, the company released its second USB 3.0 xHCI host controller (µPD720200A) and passed the compliance and certification testing in only two months. These host controllers have become the de facto USB 3.0 host controller standard realizing the best interoperability between PCs and PC peripherals that support USB 3.0.
Following these devices, two new host controllers joined the Renesas USB 3.0 product lineup in March 2011 to deliver even faster transfer speeds, better power efficiency, and more compact size than the company's previous versions of USB 3.0 host controllers.
Renesas Electronics is the world's largest producer of USB 3.0 host controllers and provides complete USB 3.0 solutions, which includes device drivers for Windows™ XP, Vista™ and Windows 7. Renesas Electronics also licenses both host and device-side USB 3.0 IP and offers USB host- and device-side building blocks within its custom ASIC libraries for companies wishing to design and market their own USB 3.0 integrated circuits.
Note: SATA (Serial ATA) is a storage interface specification that supports high-speed serial communication. It was developed for high-speed data transfers with mass storage devices such as hard-disk drives.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks)
SATA is an unregistered trademark of Serial ATA International Organization. AMD is a trademark of Advanced Micro Devices, Inc. in the United States and/or other jurisdictions Other product names and service names that appear in this press release are all trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.