Skip to main content
Renesas Electronics Corporation

Update 2 (Final) - Impact of the Instantaneous Voltage Drop on the Operation of Kawashiri Factory

July 11, 2022

Renesas today announced a final update on the impact of the production of the Kawashiri Factory (Kumamoto City, Kumamoto Prefecture) from the instantaneous voltage drop on July 5 JST caused by lightning.

We have reached full production capacity (wafer input base) equivalent to before the instantaneous voltage drop on July 11 JST, as initially scheduled.

Some damage was made to the work-in-process from the instantaneous voltage drop, and we had initially announced that losses due to ruined work-in-process and halted production may account for a maximum of approximately 2 weeks’ worth of production. However, based on further assessment, the amount of ruined work-in-process was less than anticipated, and the combined losses from ruined work-in-process and halted production will account for approximately 1 week’s worth of production. We are continuously moving forward to recover these shortfalls.