Skip to main content

Stepping Motor X Servo Control

May 26, 2020

The RENESAS + MinebeaMitsumi = 2Arms Demo features high precision and smooth position control from low speed to high speed (1 to 3000 rpm). This is a demonstration of a 2-axis robot arm using stepping motor with resolver, and was exhibited at MinebeaMitsumi's booth at International Robot Exhibition 2019.