Skip to main content

Self-capacitance Waterproof Touch Button Solution

Oct 1, 2021

The capacitive touch sensing unit "CTSU2" has enhanced noise immunity functions and supports "active shields." It is also effective in improving the water resistance of self-capacitance touch buttons. In this demo, a GND shield and an active shield have been placed to compare the water resistance of each shielding method.