Skip to main content

(6) Renesas Motor Workbench Analyzer + Tuner [Application]

Aug 4, 2022

Adjust motor control parameters by monitoring the motor’s behavior and internal variable waveform at the same time

  • Display waveforms of trigger set internal variables during motor start up
  • Confirm reference speed value and motor rotation speed
  • Change control parameters and control traceability and stability