Skip to main content

R-Car S4 SDK: Linux BSP Setup App Part 3

Aug 3, 2023

Renesas provides the R-Car S4 SDK, software that runs on the R-Car S4 SoC.

This video, Part 3 of Linux BSP setup in the 'R-Car S4 Startup Guide', explains 'Boot Kernel by using eMMC' as the following steps.

  • Prepare image, DTB files, and userland to NFS.
  • Write image files and userland to eMMC.
  • Boot Kernel for board S4 by using eMMC.