Skip to main content

How to Debug FreeRTOS Using Tracealyzer® for RX

Sep 15, 2023

This video explains the preparation to launch Tracealyzer® during application development in e2 studio for the Renesas RX Family.
See also the application note Tracealyzer® for FreeRTOS Debugging Rev1.01 (PDF | English, 日本語)

00:00 Opening
00:24 Preparing to debug FreeRTOS with Tracealyzer®
01:19 Creating a project to operate Tracealyzer® via UART
05:51 Connecting the host PC and CK-RX65N board
06:37 Starting debugging of a project with Tracealyzer®