Skip to main content

pkg_8834 (DO-41 2)

Title Information
Pkg. Name
Name used to describe Renesas packages.
GRZZ0002ZA-A
Pkg. Previous Code
Package code maintained as part of the Renesas and Intersil merger.
DO-41V
JEITA Standard
The JEITA standard to which the device is compliant.
-
Package Status
Active
Package Type
DO-41
Class
Dic
Package Code
The unique identifier of this package.
pkg_8834
Lead Count
2
Pb (Lead) Free
Yes