Skip to main content
Renesas Electronics Corporation

GR-ADZUKI Special Project: Sketch Using IDE for GR

Overview

This project describes how to create a GR-ADZUKI sketch (also called a “program”) using the IDE for GR which allows you to program using the same operations as the Arduino IDE. By downloading the IDE for GR, you can create a sketch without an internet connection.

Preparation

Hardware

You will need a GR-ADZUKI board and a USB cable (Micro B type). Make sure both slide switches on the GR-ADZUKI board are set to USB and Sketch, correspondingly.

Software

First, download IDE for GR. If using Windows, decompress the zip file. If using Mac, open the DMG file and register as an application. IDE4GR will be added to Finder as an application.

gr-adzuki-board
usb-cable

Protocol

1. Startup IDE for GR

For Windows, execute the ide4gr.exe file from the decompress folder.

For Mac, execute the IDE4GR file from the Finder application.

ide4gr-win10

2. Connect GR-ADZUKI to the PC with a USB Cable

Connect GR-ADZUKI to your computer with a USB cable. If you see a message that the USB driver cannot be located, obtain a USB driver from the FTDI website and confirm that your computer acknowledges it.

gr-adzuki-sp-connect-to-pc

3. MCU Board Selection

From the menu, select ToolsMCU BoardGR-ADZUKI.

gr-adzuki-sp-board-selection

4. Select Serial Board

From the menu, select ToolsSerial Board.

When using Windows you can confirm the port number using the device manager, or you can continue as is and change the port if an error occurs when you write the sketch to the MCU.

gr-adzuki-sp-select-serial-board

5. Loading the Sample Program

Now let’s try executing the sample program. From the menu, go to FileSketch Example03.Analog, and select “Fading.” A screen showing the written sample sketch will then be displayed.

gr-adzuki-sp-sample-program-fading

6. Compiling and Writing the Sketch

Select the arrow as is shown in the screen here. This will start compiling the program and continue on to write the program to the MCU.

If you get an error message, follow these steps:

  • Click the Write (arrow) button again. Does anything change? (A communication error message due to timing may appear if a sketch that implements serial communication has already been sent.)
  • Has the correct serial port been selected?
  • Are the GR-ADZUKI slide switches correctly set to USB and Sketch?
  • Is the USB cable firmly inserted?
gr-adzuki-sp-compiling-writing-sketch

Congratulations!

LED 9 on the GR-ADZUKI board should turn on when the Write process is complete.

Try out more samples, change the LED number, etc. Have fun!

Support

Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?