Skip to main content
Renesas Electronics Corporation

GR-PEACH Special Project: Omron HVC-P2 Human Recognition Camera Module

Part 3. Setting Up a Web Camera

Overview

In this project, we will show an image with a browser as a web camera after having detected a person with HVC-P2.

peach-sp-hvcp2-sample-face-rec


Preparation

You will need a GR-PEACH board, HVC-P2, two USB cables (Micro B type), a USB conversion adapter (Type A). Refer to the image on the right for how to connect everything together.

Prepare a Micro SD card to save the HTML file for browser indication. We will explain about the HTML file later.

peach-sp-hvcp2-prepare
peach-sp-sd-microsd

Place a short jumper (JP3) in the center part of GR-PEACH in the circuit. This allows the VBUS to receive power supply when it’s connected as a USB host.

Finally, connect an LAN cable to GR-PEACH.

peach-sp-hvcp2-prepare-board
peach-sp-hvcp2-lan-plugin

Web Camera Sample Program for Human Recognition Application

First, save the files "index.htm" and "mbedrpc.js" on the Micro SD. These files are for browser indication.

Right click the following files and execute “save an object in file", for download.

After saving, insert the Micro SD into an SD socket on the back side of GR-PEACH to build the following sketch program and write it to GR-PEACH.

Build the following sample program with a web compiler, and write down a bin file to GR-PEACH. Double-click on a source, whole document will be selected.


/* GR-PEACH Sketch Template for using HVC-P2
 * based on library version V1.06
 */
 
// GR-PEACH API
#include <Arduino.h>
#include <SD.h>
#include <EthernetInterface.h>
#include <HTTPServer.h>
#include <mbed_rpc.h>
#include <RomRamFileSystem.h>
#include <USBHostSerial.h>
#include <JPEG_Converter.h>
// HVC-P2 API
#include "HVCApi.h" // Omron sample
#include "HVCDef.h" // Omron sample
#include "HVCExtraUartFunc.h" // Omron sample
 
#define USB_SETTING_TIMEOUT 1000
#define USB_EXECUTE_TIMEOUT 2000
//#define ALL_DETECTION
#define SENSOR_ROLL_ANGLE_DEFAULT            0            /* Camera angle setting (0°) */
#define BODY_THRESHOLD_DEFAULT             500            /* Threshold for Human Body Detection */
#define FACE_THRESHOLD_DEFAULT             500            /* Threshold for Face Detection */
#define HAND_THRESHOLD_DEFAULT             500            /* Threshold for Hand Detection */
#define REC_THRESHOLD_DEFAULT              500            /* Threshold for Face Recognition */
#define BODY_SIZE_RANGE_MIN_DEFAULT         30            /* Human Body Detection minimum detection size */
#define BODY_SIZE_RANGE_MAX_DEFAULT       8192            /* Human Body Detection maximum detection size */
#define HAND_SIZE_RANGE_MIN_DEFAULT         40            /* Hand Detection minimum detection size */
#define HAND_SIZE_RANGE_MAX_DEFAULT       8192            /* Hand Detection maximum detection size */
#define FACE_SIZE_RANGE_MIN_DEFAULT         64            /* Face Detection minimum detection size */
#define FACE_SIZE_RANGE_MAX_DEFAULT       8192            /* Face Detection maximum detection size */
#define FACE_POSE_DEFAULT                    0            /* Face Detection facial pose (frontal face)*/
#define FACE_ANGLE_DEFAULT                   0            /* Face Detection roll angle (±15°)*/
#define PIXEL_WIDTH                 (320)
#define PIXEL_HEIGHT                (240)
#define BYTE_PER_PIXEL_YUV   (2u)
#define BYTE_PER_PIXEL_RGB   (3u)
#define FRAME_STRIDE_YUV   (((PIXEL_WIDTH * BYTE_PER_PIXEL_YUV) + 31u) & ~31u)
#define FRAME_STRIDE_RGB   (((PIXEL_WIDTH * BYTE_PER_PIXEL_RGB) + 31u) & ~31u)
#define NUM_WEBFILES 2
 
/*! Frame buffer stride: Frame buffer stride should be set to a multiple of 32 or 128
 in accordance with the frame buffer burst transfer mode. */
static uint8_t frame_buffer_YUV422[FRAME_STRIDE_YUV * PIXEL_HEIGHT]__attribute((section("NC_BSS"),aligned(32)));
static uint8_t frame_buffer_RGB888[FRAME_STRIDE_RGB * PIXEL_HEIGHT]__attribute((section("NC_BSS"),aligned(32)));
static uint8_t JpegBuffer[1024 * 200]__attribute((aligned(8))); //8 bytes aligned!;
static volatile int jcu_encoding = 1;
static volatile int jcu_encode_size = 1;
static JPEG_Converter Jcu;
static EthernetInterface network;
static RomRamFileSystem romramfs("romram");
const char mount_files[NUM_WEBFILES][13] = { //name should be 8.3 format
        "index.htm", "mbedrpc.js" };
File myFile;
void RPC_HVC_Read(Arguments* arg, Reply* r);
void RPC_HVC_Write(Arguments* arg, Reply* r);
int char_to_int(char* c, int len);
static USBHostSerial * p_cdc;
extern "C" int UART_SendData(int inDataSize, UINT8 *inData) {
    return p_cdc->writeBuf((char *) inData, inDataSize);
}
extern "C" int UART_ReceiveData(int inTimeOutTime, int inDataSize,
        UINT8 *outResult) {
    return p_cdc->readBuf((char *) outResult, inDataSize, inTimeOutTime);
}
static bool hvc_rec_face = true;
static bool hvc_rec_age = false;
static bool hvc_rec_gender = false;
static bool hvc_rec_gaze = false;
static bool hvc_rec_blink = false;
static bool hvc_rec_expression = false;
static bool hvc_rec_body = false;
static bool hvc_rec_hand = false;
static int hvc_age;
static int hvc_gender;
static int hvc_gaze_lr;
static int hvc_gaze_ud;
static int hvc_blink_l;
static int hvc_blink_r;
static int hvc_expression;
static int hvc_resolution = HVC_EXECUTE_IMAGE_QVGA;
static int hvc_pixel_width = PIXEL_WIDTH;
static int hvc_pixel_height = PIXEL_HEIGHT;
 
void led_blink(int pin, int num) {
    for (int i = 0; i < num; i++) {
        digitalWrite(pin, HIGH);
        delay(50);
        digitalWrite(pin, LOW);
        delay(50);
    }
}
static void EraseImage(uint8_t* buf, uint32_t size) {
    uint32_t i = 0;
    while (i < size) {
        buf[i++] = 0x10;
        buf[i++] = 0x80;
    }
}
 
static void dcache_invalid(void * p_buf, uint32_t size) {
    uint32_t start_addr = (uint32_t) p_buf & 0xFFFFFFE0;
    uint32_t end_addr = (uint32_t) p_buf + size;
    uint32_t addr;
 
    // Data cache invalid
    for (addr = start_addr; addr < end_addr; addr += 0x20) {
        __v7_inv_dcache_mva((void *) addr);
    }
}
 
void JcuEncodeCallBackFunc(JPEG_Converter::jpeg_conv_error_t err_code) {
    jcu_encoding = 0;
}
 
size_t JpegEncode(uint8_t* buf, int len, int width, int height, uint8_t* inbuf) {
    size_t encode_size;
    JPEG_Converter::bitmap_buff_info_t bitmap_buff_info;
    JPEG_Converter::encode_options_t encode_options;
    bitmap_buff_info.width = width;
    bitmap_buff_info.height = height;
    bitmap_buff_info.format = JPEG_Converter::WR_RD_YCbCr422;
    bitmap_buff_info.buffer_address = (void *) inbuf;
    encode_options.encode_buff_size = sizeof(buf);
    encode_options.p_EncodeCallBackFunc = &JcuEncodeCallBackFunc;
    //    encode_options.input_swapsetting = JPEG_Converter::WR_RD_WRSWA_32_16_8BIT;
 
    jcu_encoding = 1; // flag for waiting callback function of JCU
    jcu_encode_size = 0;
    dcache_invalid(buf, len);
    if (Jcu.encode(&bitmap_buff_info, buf, &encode_size, &encode_options)
            != JPEG_Converter::JPEG_CONV_OK) {
        jcu_encode_size = 0;
        jcu_encoding = 0;
    }
 
    while (jcu_encoding == 1) {
        delay(1);
    }
 
    return encode_size;
}
static void DrawSquare(int x, int y, int size, uint32_t const colour, uint8_t* inbuf) {
    int wk_x;
    int wk_y;
    int wk_w = 0;
    int wk_h = 0;
    int idx_base;
    int wk_idx;
    int i;
    int j;
    uint8_t coller_pix[BYTE_PER_PIXEL_RGB];
    bool l_draw = true;
    bool r_draw = true;
    bool t_draw = true;
    bool b_draw = true;
 
    if ((x - (size / 2)) < 0) {
        l_draw = false;
        wk_w += x;
        wk_x = 0;
    } else {
        wk_w += (size / 2);
        wk_x = x - (size / 2);
    }
 
    if ((x + (size / 2)) >= 1600) {
        r_draw = false;
        wk_w += (1600 - x);
    } else {
        wk_w += (size / 2);
    }
 
    if ((y - (size / 2)) < 0) {
        t_draw = false;
        wk_h += y;
        wk_y = 0;
    } else {
        wk_h += (size / 2);
        wk_y = y - (size / 2);
    }
 
    if ((y + (size / 2)) >= 1200) {
        b_draw = false;
        wk_h += (1200 - y);
    } else {
        wk_h += (size / 2);
    }
 
    wk_x = wk_x / 5 / hvc_resolution;
    wk_y = wk_y / 5 / hvc_resolution;
    wk_w = wk_w / 5 / hvc_resolution;
    wk_h = wk_h / 5 / hvc_resolution;
 
    idx_base = (wk_x + (hvc_pixel_width * wk_y)) * BYTE_PER_PIXEL_RGB;
 
    /* Select color */
    coller_pix[0] = (colour >> 16) & 0xff;
    coller_pix[1] = (colour >> 8) & 0xff;
    coller_pix[2] = colour & 0xff;
 
    /* top */
    if (t_draw) {
        wk_idx = idx_base;
        for (j = 0; j < wk_w; j++) {
            inbuf[wk_idx++] = coller_pix[0];
            inbuf[wk_idx++] = coller_pix[1];
            inbuf[wk_idx++] = coller_pix[2];
        }
    }
 
    /* middle */
    for (i = 1; i < (wk_h - 1); i++) {
        wk_idx = idx_base + (hvc_pixel_width * BYTE_PER_PIXEL_RGB * i);
        if (l_draw) {
            inbuf[wk_idx + 0] = coller_pix[0];
            inbuf[wk_idx + 1] = coller_pix[1];
            inbuf[wk_idx + 2] = coller_pix[2];
        }
        wk_idx += (wk_w - 1) * 3;
        if (r_draw) {
            inbuf[wk_idx + 0] = coller_pix[0];
            inbuf[wk_idx + 1] = coller_pix[1];
            inbuf[wk_idx + 2] = coller_pix[2];
        }
    }
 
    /* bottom */
    if (b_draw) {
        wk_idx = idx_base + (hvc_pixel_width * BYTE_PER_PIXEL_RGB * (wk_h - 1));
        for (j = 0; j < wk_w; j++) {
            inbuf[wk_idx++] = coller_pix[0];
            inbuf[wk_idx++] = coller_pix[1];
            inbuf[wk_idx++] = coller_pix[2];
        }
    }
}
 
static int snapshot_req(const char ** pp_data) {
    INT32 timeOutTime;
    int encode_size;
    INT32 execFlag;
    timeOutTime = USB_EXECUTE_TIMEOUT;
    INT32 ret = 0; /* Return code */
    UINT8 status;
    HVC_RESULT *pHVCResult = NULL;
    HVC_IMAGE *pImage = NULL;
 
    /*********************************/
    /* Result Structure Allocation   */
    /*********************************/
    pHVCResult = (HVC_RESULT *) malloc(sizeof(HVC_RESULT));
    if (pHVCResult == NULL) { /* Error processing */
        Serial.println("Memory Allocation Error");
        mbed_die();
    }
 
    /* Image Structure allocation */
    pImage = (HVC_IMAGE *) malloc(sizeof(HVC_IMAGE));
    if (pImage == NULL) {
        printf("Memory Allocation Error : %08x\n", sizeof(HVC_RESULT));
        mbed_die();
    }
    execFlag = 0;
    if(hvc_rec_face == true){
        execFlag |= (HVC_ACTIV_FACE_DETECTION | HVC_ACTIV_FACE_DIRECTION);
    }
    if(hvc_rec_age == true){
        execFlag |= HVC_ACTIV_AGE_ESTIMATION;
    }
    if(hvc_rec_gender == true){
        execFlag |= HVC_ACTIV_GENDER_ESTIMATION;
    }
    if(hvc_rec_gaze == true){
        execFlag |= HVC_ACTIV_GAZE_ESTIMATION;
    }
    if(hvc_rec_blink == true){
        execFlag |= HVC_ACTIV_BLINK_ESTIMATION;
    }
    if(hvc_rec_expression == true){
        execFlag |= HVC_ACTIV_EXPRESSION_ESTIMATION;
    }
    if(hvc_rec_body == true){
        execFlag |= HVC_ACTIV_BODY_DETECTION;
    }
    if(hvc_rec_hand == true){
        execFlag |= HVC_ACTIV_HAND_DETECTION;
    }
    ret = HVC_ExecuteEx(timeOutTime, execFlag, hvc_resolution,
            pHVCResult, &status);
    if ((ret != 0) || (status != 0)) {
        Serial.println("HVC_ExecuteEx Error");
    }
    EraseImage(frame_buffer_YUV422, sizeof(frame_buffer_YUV422));
 
    // Prepare image data
    // HVC-P2 outputs Y in order 4-3-2-1
    // To simplify data processing, convert from 4-3-2-1 to 1-2-3-4
    for (int i = 0; i < hvc_pixel_height; i++){
        for (int j = 0; j < (hvc_pixel_width / 4); j++){
            uint8_t temp[4];
            temp[0] = pHVCResult->image.image[i * hvc_pixel_width + j * 4 + 3];
            temp[1] = pHVCResult->image.image[i * hvc_pixel_width + j * 4 + 2];
            temp[2] = pHVCResult->image.image[i * hvc_pixel_width + j * 4 + 1];
            temp[3] = pHVCResult->image.image[i * hvc_pixel_width + j * 4 + 0];
            pHVCResult->image.image[i * hvc_pixel_width + j * 4 + 0] = temp[0];
            pHVCResult->image.image[i * hvc_pixel_width + j * 4 + 1] = temp[1];
            pHVCResult->image.image[i * hvc_pixel_width + j * 4 + 2] = temp[2];
            pHVCResult->image.image[i * hvc_pixel_width + j * 4 + 3] = temp[3];
        }
    }
 
    for (int i = 0; i < hvc_pixel_height; i++) {
        for (int j = 0; j < hvc_pixel_width; j++) {
            uint8_t Y = pHVCResult->image.image[i * hvc_pixel_width + j];
            for (int k = 0; k < 3; k++){
                frame_buffer_RGB888[(i * hvc_pixel_width * BYTE_PER_PIXEL_RGB)
                        + BYTE_PER_PIXEL_RGB * j + k] = Y;
            }
        }
    }
 
    if(pHVCResult->bdResult.num | pHVCResult->hdResult.num | pHVCResult->fdResult.num){
        led_blink(PIN_LED_BLUE, 2);
#if 0 // Y to YUV422
        for (int i = 0; i < hvc_pixel_height; i++) {
            for (int j = 0; j < (hvc_pixel_width); j++) {
                frame_buffer_YUV422[(i * hvc_pixel_width * BYTE_PER_PIXEL_YUV)
                        + BYTE_PER_PIXEL_YUV * j] = pHVCResult->image.image[i * hvc_pixel_width + j];
            }
        }
#endif
 
    }
    if(pHVCResult->executedFunc & HVC_ACTIV_BODY_DETECTION){
        /* Body Detection result string */
        Serial.print("Body result count:"); Serial.println(pHVCResult->bdResult.num);
        for(int i = 0; i < pHVCResult->bdResult.num; i++){

            // Draw red square
            DrawSquare(pHVCResult->bdResult.bdResult[i].posX,
                       pHVCResult->bdResult.bdResult[i].posY,
                       pHVCResult->bdResult.bdResult[i].size,
                       0x00f00000, frame_buffer_RGB888);
        }
    }
    if(pHVCResult->executedFunc & HVC_ACTIV_HAND_DETECTION){
        /* Hand Detection result string */
        Serial.print("Hand result count:"); Serial.println(pHVCResult->hdResult.num);
        for(int i = 0; i < pHVCResult->hdResult.num; i++){
            // Draw yellow square
            DrawSquare(pHVCResult->hdResult.hdResult[i].posX,
                       pHVCResult->hdResult.hdResult[i].posY,
                       pHVCResult->hdResult.hdResult[i].size,
                       0x00f0f000, frame_buffer_RGB888);
        }
    }
    /* Face Detection result string */
    if(pHVCResult->executedFunc & HVC_ACTIV_FACE_DETECTION){
        Serial.print("Face result count:"); Serial.println(pHVCResult->fdResult.num);
        for(int i = 0; i < pHVCResult->fdResult.num; i++){
            if(pHVCResult->executedFunc & HVC_ACTIV_FACE_DETECTION){
                /* Detection */
                // Draw sky blue square
                DrawSquare(pHVCResult->fdResult.fcResult[i].dtResult.posX,
                           pHVCResult->fdResult.fcResult[i].dtResult.posY,
                           pHVCResult->fdResult.fcResult[i].dtResult.size,
                           0x00ffffff, frame_buffer_RGB888);
            }
            if(pHVCResult->executedFunc & HVC_ACTIV_FACE_DIRECTION){
                /* Face Direction */
            }
            if(pHVCResult->executedFunc & HVC_ACTIV_AGE_ESTIMATION){
                /* Age */
                hvc_age = pHVCResult->fdResult.fcResult[0].ageResult.age;
            }
            if(pHVCResult->executedFunc & HVC_ACTIV_GENDER_ESTIMATION){
                /* Gender */
                if(-128 == pHVCResult->fdResult.fcResult[i].genderResult.gender){
                    // do nothing
                }
                else{
                    hvc_gender = pHVCResult->fdResult.fcResult[0].genderResult.gender;
                    if(1 == pHVCResult->fdResult.fcResult[i].genderResult.gender){
                        // Draw sky blue square
                        DrawSquare(pHVCResult->fdResult.fcResult[i].dtResult.posX,
                                   pHVCResult->fdResult.fcResult[i].dtResult.posY,
                                   pHVCResult->fdResult.fcResult[i].dtResult.size,
                                   0x0000f0f0, frame_buffer_RGB888);
                    }
                    else{
                        // Draw pink square
                        DrawSquare(pHVCResult->fdResult.fcResult[i].dtResult.posX,
                                   pHVCResult->fdResult.fcResult[i].dtResult.posY,
                                   pHVCResult->fdResult.fcResult[i].dtResult.size,
                                   0x00f000f0, frame_buffer_RGB888);
                    }
                }
            }
            if(pHVCResult->executedFunc & HVC_ACTIV_GAZE_ESTIMATION){
                /* Gaze */
                if((-128 == pHVCResult->fdResult.fcResult[i].gazeResult.gazeLR) ||
                    (-128 == pHVCResult->fdResult.fcResult[i].gazeResult.gazeUD)){
                    // do nothing
                }
                else{
                    hvc_gaze_lr = pHVCResult->fdResult.fcResult[0].gazeResult.gazeLR;
                    hvc_gaze_ud = pHVCResult->fdResult.fcResult[0].gazeResult.gazeUD;
                }
            }
            if(pHVCResult->executedFunc & HVC_ACTIV_BLINK_ESTIMATION){
                /* Blink */
                hvc_blink_l = pHVCResult->fdResult.fcResult[0].blinkResult.ratioL;
                hvc_blink_r = pHVCResult->fdResult.fcResult[0].blinkResult.ratioR;
            }
            if(pHVCResult->executedFunc & HVC_ACTIV_EXPRESSION_ESTIMATION){
                /* Expression */
                hvc_expression = pHVCResult->fdResult.fcResult[0].expressionResult.topExpression;
            }
        }
    }
 
    for (int i = 0; i < hvc_pixel_height; i++) {
        for (int j = 0; j < hvc_pixel_width; j+=2) { // processing 2 pixels
            uint8_t r0,g0,b0,r1,g1,b1,y0,y1,u,v;
            r1 = frame_buffer_RGB888[(i * hvc_pixel_width * BYTE_PER_PIXEL_RGB)
                    + BYTE_PER_PIXEL_RGB * j + 5];
            g1 = frame_buffer_RGB888[(i * hvc_pixel_width * BYTE_PER_PIXEL_RGB)
                    + BYTE_PER_PIXEL_RGB * j + 4];
            b1 = frame_buffer_RGB888[(i * hvc_pixel_width * BYTE_PER_PIXEL_RGB)
                    + BYTE_PER_PIXEL_RGB * j + 3];
            r0 = frame_buffer_RGB888[(i * hvc_pixel_width * BYTE_PER_PIXEL_RGB)
                    + BYTE_PER_PIXEL_RGB * j + 2];
            g0 = frame_buffer_RGB888[(i * hvc_pixel_width * BYTE_PER_PIXEL_RGB)
                    + BYTE_PER_PIXEL_RGB * j + 1];
            b0 = frame_buffer_RGB888[(i * hvc_pixel_width * BYTE_PER_PIXEL_RGB)
                    + BYTE_PER_PIXEL_RGB * j + 0];
 
            y0 = round( 0.256788 * r0 + 0.504129 * g0 + 0.097906 * b0) +  16;
            y1 = round( 0.256788 * r1 + 0.504129 * g1 + 0.097906 * b1) +  16;
            if(r0!=g0){ // it's not gray that means color line
                u = round(-0.148223 * r0 - 0.290993 * g0 + 0.439216 * b0) + 128;
                v = round( 0.439216 * r0 - 0.367788 * g0 - 0.071427 * b0) + 128;
            } else if (r1!=g1){ // it's not gray that means color line
                u = round(-0.148223 * r1 - 0.290993 * g1 + 0.439216 * b1) + 128;
                v = round( 0.439216 * r1 - 0.367788 * g1 - 0.071427 * b1) + 128;
            } else { // it's gray.
                u = round(-0.148223 * r0 - 0.290993 * g0 + 0.439216 * b0) + 128;
                v = round( 0.439216 * r0 - 0.367788 * g0 - 0.071427 * b0) + 128;
            }
 
            frame_buffer_YUV422[(i * hvc_pixel_width * BYTE_PER_PIXEL_YUV)
                    + BYTE_PER_PIXEL_YUV * j + 0] = y0;
            frame_buffer_YUV422[(i * hvc_pixel_width * BYTE_PER_PIXEL_YUV)
                    + BYTE_PER_PIXEL_YUV * j + 1] = u;
            frame_buffer_YUV422[(i * hvc_pixel_width * BYTE_PER_PIXEL_YUV)
                    + BYTE_PER_PIXEL_YUV * j + 2] = y1;
            frame_buffer_YUV422[(i * hvc_pixel_width * BYTE_PER_PIXEL_YUV)
                    + BYTE_PER_PIXEL_YUV * j + 3] = v;
        }
    }
    encode_size = JpegEncode(JpegBuffer, sizeof(JpegBuffer), hvc_pixel_width, hvc_pixel_height, frame_buffer_YUV422);
    *pp_data = (const char *) JpegBuffer;
 
    free(pHVCResult);
    free(pImage);
    return encode_size;
}
 
int char_to_int(char* c, int len){
    int r = 0;
    for (int i = 0; i < len; i++) {
        if (c[i] == 0) break;
        r = r * 10 + c[i] - '0';
    }
    return r;
 
}
void RPC_HVC_Read(Arguments* arg, Reply* r){
 
    int ret;
    char rpc_hvc_read_buf[10];
    const char *pExStr[] = { "?", "Neutral", "Happiness", "Surprise", "Anger",
            "Sadness" };
 
    if (arg != NULL) {
 
        switch(char_to_int(arg->argv[0], 2)){
        case 0:
            sprintf(rpc_hvc_read_buf, "%d", hvc_age);
            break;
        case 1:
            if(hvc_gender == 1){
                sprintf(rpc_hvc_read_buf, "Male");
            } else {
                sprintf(rpc_hvc_read_buf, "Female");
            }
            break;
        case 2:
            ret = hvc_gaze_lr;
            sprintf(rpc_hvc_read_buf, "%d", ret);
            break;
        case 3:
            ret = hvc_gaze_ud;
            sprintf(rpc_hvc_read_buf, "%d", ret);
            break;
        case 4:
            ret = hvc_blink_l;
            sprintf(rpc_hvc_read_buf, "%d", ret);
            break;
        case 5:
            ret = hvc_blink_r;
            sprintf(rpc_hvc_read_buf, "%d", ret);
            break;
        case 6:
            ret = hvc_expression;
            sprintf(rpc_hvc_read_buf, "%s", pExStr[hvc_expression]);

            break;
        }
 
        /* command analysis and execute */
        r->putData<const char*>(rpc_hvc_read_buf);
        //delay(1);
    }
}
void RPC_HVC_Write(Arguments* arg, Reply* r) {
    Serial.println(char_to_int(arg->argv[0], 1));
    Serial.println(char_to_int(arg->argv[1], 1));
    if (arg != NULL) {
        /* command analysis and execute */
        if(char_to_int(arg->argv[0], 1) == 0){ // modify resolution
            if(char_to_int(arg->argv[1], 1) == 1){
                hvc_resolution = HVC_EXECUTE_IMAGE_QVGA;
                hvc_pixel_width = PIXEL_WIDTH;
                hvc_pixel_height = PIXEL_HEIGHT;
            } else {
                hvc_resolution = HVC_EXECUTE_IMAGE_QVGA_HALF;
                hvc_pixel_width = PIXEL_WIDTH / 2;
                hvc_pixel_height = PIXEL_HEIGHT / 2;
            }
        } else if(char_to_int(arg->argv[0], 1) == 1){ // enable each estimation
            switch(char_to_int(arg->argv[1], 1)){
            case 0:
                hvc_rec_face = true;
                break;
            case 1:
                hvc_rec_age = true;
                break;
            case 2:
                hvc_rec_gender = true;
                break;
            case 3:
                hvc_rec_gaze = true;
                break;
            case 4:
                hvc_rec_blink = true;
                break;
            case 5:
                hvc_rec_expression = true;
                break;
            case 6:
                hvc_rec_body = true;
                break;
            case 7:
                hvc_rec_hand = true;
                break;
            }
        } else if(char_to_int(arg->argv[0], 1) == 2){ // enable each estimation
            switch(char_to_int(arg->argv[1], 1)){
            case 0:
                hvc_rec_face = false;
                break;
            case 1:
                hvc_rec_age = false;
                break;
            case 2:
                hvc_rec_gender = false;
                break;
            case 3:
                hvc_rec_gaze = false;
                break;
            case 4:
                hvc_rec_blink = false;
                break;
            case 5:
                hvc_rec_expression = false;
                break;
            case 6:
                hvc_rec_body = false;
                break;
            case 7:
                hvc_rec_hand = false;
                break;
            }
        }
        led_blink(PIN_LED_RED, 1);
    }
}
static void mount_romramfs(void) {
    FILE * fp;
    romramfs.format();
 
    char write_path[20];
 
    for (int i = 0; i < NUM_WEBFILES; i++) {
        myFile = SD.open(mount_files[i], FILE_READ);
        if (myFile) {
            sprintf(write_path, "/romram/%s", mount_files[i]);
            fp = fopen(write_path, "w");
            // read from the file until there's nothing else in it:
            while (myFile.available()) {
                putc(myFile.read(), fp);
            }
            // close the file:
            myFile.close();
            fclose(fp);
        }
    }
}
void setup() {
    INT32 ret = 0; /* Return code */
    UINT8 status;
 
    INT32 agleNo;
    HVC_THRESHOLD threshold;
    HVC_SIZERANGE sizeRange;
    INT32 pose;
    INT32 angle;
 
    pinMode(PIN_LED_RED, OUTPUT);
    pinMode(PIN_LED_GREEN, OUTPUT);
    pinMode(PIN_LED_BLUE, OUTPUT);
 
    Serial.begin(9600);
    Serial.println("Program starts");
 
    USBHostSerial cdc;
    p_cdc = &cdc; // for HVC P2 API
 
    Serial.println("SD Setting up...");
    if (!SD.begin()) {
        Serial.println("initialization failed!");
        return;
    }
    mount_romramfs();   //RomRamFileSystem Mount
    RPCFunction rpc_hvc_read(&RPC_HVC_Read, "RPC_HVC_Read");
    RPCFunction rpc_rpc_hvc_read(&RPC_HVC_Write, "RPC_HVC_Write");
    Serial.println("done.");
 
 
    Serial.println("Network Setting up...");
    if (network.init() != 0) {                             //for DHCP Server
    //if (network.init(IP_ADDRESS, SUBNET_MASK, DEFAULT_GATEWAY) != 0) { //for Static IP Address (IPAddress, NetMasks, Gateway)
        return;
    }
    if (network.connect() != 0) {
        return;
    }
 
    Serial.print("MAC Address is ");
    Serial.println(network.getMACAddress());
    Serial.print("IP Address is ");
    Serial.println(network.getIPAddress());
    Serial.print("NetMask is ");
    Serial.println(network.getNetworkMask());
    Serial.print("Gateway Address is ");
    Serial.println(network.getGateway());
    Serial.println("Network Setup OK");
 
    Serial.print("Waiting USB device...");
 
    while (!p_cdc->connect()) { // wait for connecting HVC
        led_blink(PIN_LED_RED, 1);
        Thread::wait(500);
    }
    Serial.println("found.");
 
    led_blink(PIN_LED_GREEN, 2);
    p_cdc->baud(921600);
 
    /*********************************/
    /* Set Camera Angle              */
    /*********************************/
    agleNo = SENSOR_ROLL_ANGLE_DEFAULT;
    ret = HVC_SetCameraAngle(USB_SETTING_TIMEOUT, agleNo, &status);
    /*********************************/
    /* Set Threshold Values          */
    /*********************************/
    threshold.bdThreshold = BODY_THRESHOLD_DEFAULT;
    threshold.hdThreshold = HAND_THRESHOLD_DEFAULT;
    threshold.dtThreshold = FACE_THRESHOLD_DEFAULT;
    threshold.rsThreshold = REC_THRESHOLD_DEFAULT;
    ret = HVC_SetThreshold(USB_SETTING_TIMEOUT, &threshold, &status);
    /*********************************/
    /* Set Detection Size            */
    /*********************************/
    sizeRange.bdMinSize = BODY_SIZE_RANGE_MIN_DEFAULT;
    sizeRange.bdMaxSize = BODY_SIZE_RANGE_MAX_DEFAULT;
    sizeRange.hdMinSize = HAND_SIZE_RANGE_MIN_DEFAULT;
    sizeRange.hdMaxSize = HAND_SIZE_RANGE_MAX_DEFAULT;
    sizeRange.dtMinSize = FACE_SIZE_RANGE_MIN_DEFAULT;
    sizeRange.dtMaxSize = FACE_SIZE_RANGE_MAX_DEFAULT;
    ret = HVC_SetSizeRange(USB_SETTING_TIMEOUT, &sizeRange, &status);
    /*********************************/
    /* Set Face Angle                */
    /*********************************/
    pose = FACE_POSE_DEFAULT;
    angle = FACE_ANGLE_DEFAULT;
    ret = HVC_SetFaceDetectionAngle(USB_SETTING_TIMEOUT, pose, angle, &status);
 
    SnapshotHandler::attach_req(&snapshot_req);
    HTTPServerAddHandler<SnapshotHandler>("/camera"); //Camera
    FSHandler::mount("/romram", "/");
    HTTPServerAddHandler<FSHandler>("/");
    HTTPServerAddHandler<RPCHandler>("/rpc");
    HTTPServerStart(80);
 
    while (1)
        ;
 
}
 
void loop() {
}



Operation Check for the Web Camera

After writing down a bin file, start a serial monitor such as Tera Term and then press a reset button of GR-PEACH.

As a program starts, the reading of the content on the SD card, recognition of the USB device (HVC-P2), and the network setting come through.

Then, the IP address of the LAN acquired by DHCP will be shown.

peach-sp-hvcp2-ip-add-monitor

Put an acquired IP address into the URL of the web browser. The screen of the web camera will be displayed as shown here.

In this default program, please note that only the face has been selected for detection.

peach-sp-hvcp2-sample-face-rec