Skip to main content

Sensory TrulyHandsfree Voice Control

Overview

Description

Introduced in 2009, TrulyHandsfree paved the way for the hands-free operation we have come to expect with today's always-listening personal assistant solutions. When first released it revolutionized voice user interfaces by offering the first commercially successful embedded small vocabulary speech recognition system to feature an always-listening wake word. With each succeeding generation, TrulyHandsfree has continually upped the benchmark for always-listening speech recognition performance. The current generation of TrulyHandsfree incorporates Sensory's smartest and most efficient deep neural network technologies to date, delivering an unrivaled user experience and class-leading voice interface. TrulyHandsfree offers complete scalability for deployment on ultra-low power digital signal processors (DSPs) to the most powerful applications processors available. And since all of Sensory's AI is processed on the device and not the cloud, user data stays safe and secure.

For more information, contact Shinko Shoji Co., Ltd. (Device & Solutions Engineering Dept.) in Japan. (e-mail: [email protected], TEL: +81-3-6361-8095)

Comparison

Applications