Skip to main content

Overview

Description

  • The practice of publishing separate e2 studio releases for Synergy has been discontinued. For SSP 2.0.0 and future SSP releases, users will be requested to use the Platform installer to install e2 studio and SSP together. The Platform installer for SSP 2.0.0 and future releases is available from the download page for SSP.
  • It is strongly recommended that users do not use the older versions of e2 studio for SSP 2.0.0 and future releases as these combinations have not been tested and are not supported.
  • For additional support or to request an older version of SSP or e2 studio for Synergy, users should submit a ticket through the Renesas Knowledge Base.

Target Devices