Skip to main content

NOTICE - This software / tool has been discontinued. Please contact technical support with any questions.

NOTICE - The following device(s) are recommended alternatives:
PG-FP6

Overview

Description

The PG-FP5 installed in a system is a tool for erasing, programming, and verifying programs on Renesas MCUs with on-chip flash memory.

Topics

The PG-FP5 has been discontinued. The acceptance of final orders was in May 2018. If adopting new products, please consider the successor, the PG-FP6.
[PG-FP6] Higher productivity and security than its predecessor, PG-FP5 >>

Successor

PG-FP6

Note: the PG-FP6 does not support V850 and 78K with dual power supply flash memory, which assume mass production with mask ROM. Use programmers produced by partners for programming of the V850 and 78K with dual power supply flash memory. Refer to Function and performance comparisons between PG-FP6 and PG-FP5 >>

Features

  • Standalone programming
  • PC-controlled programming using dedicated GUI
  • Ability to store settings for up to eight programming environments
  • Designed specifically for use on production lines (command control or remote control)
  • Programming a unique code to a designated area of flash memory
  • Security setting can be changed with the the Manager function
  • Supports self-testing function
  • Learn More

Release Information

Programming GUI

Latest Ver.: V2.17

Released: Apr 22, 2019

Download

Firmware

Latest Ver.: V2.17

Released: Apr 22, 2019

Download

FPGA

Latest Ver.: V4

Released: Jul 15, 2011

Download

Parameter Files

Latest file released: Apr 20, 2022

Download

Details of upgrade(See Tool News)

Operating Environment

How to find the version number

Target Family

For details of support for individual device part numbers, see List of MCUs supported by PG-FP5 (PDF | English, 日本語) (incl. information on components and parameter files).

 

Target Devices

Downloads

Documentation

Additional Details

Control panel suitable for the stand-alone operation

Image
pgfp5-syomen-e

Easy-to-Use Graphical User Interface (GUI)

Image
pgfp5-gui-e

Major Functions

  • Downloading and uploading program files and parameter files
  • Editing program files (by using HEX editor)
  • Checksum calculation
  • Saving the action logs
  • Manager function (Prohibition of uploading program files and changing the password and settings, etc.)
  • Feasibility of blank checking, erasing, programming, verifying, reading, settings and obtainment of Flash options information, checksum and programming after erasing
  • Execution of self-testing function
  • Writing in the minimum unit of the flash memory is available for the following devices
    • RX family
    • RH850 family (excluding the RH850/P1x-C group)
    • V850 family (V850E2/Fx4-L, V850/FF4-G, V850E2/FG4-G, V850E2/Px4-L, or V850PG4-S only)

Components

  • PG-FP5
  • USB cable
  • Serial cable
  • Target cables of two sorts (14-pin and 16-pin types)
  • GND cable
  • Setup manual

Note: Except for Europe, the power supply adapter, QB-COMMON-PW-xx, is not bundled in the product package of PG-FP5. Please purchase it separately.

System Configuration

Image
pgfp5-system-config

PG-FP5 How to Find the Version Number

Programming GUI, Firmware and FPGA for PG-FP5

To check the version number, follow these steps:

Step1. PG-FP5 Startup
After the cables are connected, press the POWER button on the PG-FP5.
Step2. Startup of Programming GUI
Click the Start menu, "All Programs", point to "Renesas Electronics Utilities", "Programming Tools", and then select "PG-FP5 Vx.xx" of "PG-FP5 Vx.xx" to start the Programming GUI. When communication is established and the programming GUI is correctly started, the main window will be opened.
Step3. Check the Version Numbers of the Programming GUI, Firmware and FPGA with "Reset Command" or "Main Window", as Shown Below:
  • Programming GUI
    • - Open the Help menu and click the About FP5 command.
      The version number of Programming GUI is displayed in the About FP5 dialog box.
      or
      - Refer to the programming parameter window on the right of the main window. The version number of Programming GUI is shown at the FP5_GUI row in the Programmer box of the programming parameter window.
  • Firmware
    • - Open the Programmer menu and click the Reset command.
      The version number of Firmware is displayed in the action log window.
      or
      Refer to the programming parameter window on the right of the main window. The version number of Firmware is shown at the Firmware row in the Programmer box of the programming parameter window.
  • FPGA
    • - Open the Programmer menu and click the Reset command. The version number of FPGA is displayed in the action log window.
Image
pgfp5-version-display

Display Example of Reset Command
 
Image
pgfp5-version-reset

Display Example of Main Window