Skip to main content

Migration from V2 to V3 of the Renesas Flash Programmer

Renesas Flash Programmer (Programming GUI)

Migrating from V2 to V3 of the Renesas Flash Programmer

V3 of the Renesas Flash Programmer is easier to use and provides faster programming than V2.
We recommend using V3 of the Renesas Flash Programmer for programming RH850, RX, or RL78 devices.
If you have a license for V2, you can upgrade it to V3 free of charge.

A license for V3 is also valid for V2

If you have a license for Renesas Flash Programmer V3, you can also use V2.

Providing the Renesas Flash Programmer without a physical medium

With the intention of producing more environmentally friendly products, we no longer provide the Renesas Flash Programmer on a CD-ROM as the medium following the release of V3.09.00 in October 2021. We also ended the provision of a license file that had been included on each CD-ROM. Accordingly, the Renesas Flash Programmer no longer has the feature for registration by loading a license file.
Although V3.09.00 and later versions of the Renesas Flash Programmer do not include license files, you can still get technical support as before by entering the PID number indicated in the license certificate that comes with the product.
 

Comparison Between V3 and V2 Functions

Functions Renesas Flash Programmer V2 Renesas Flash Programmer V3 Remarks
Creating Projects lens lens
Easier than V2
 
High-Speed Writing lens lens
Easier than V2
 
Cooperation With Other Software Through Batch Processing lens Note 1 lens Note 2  
Checksums of Program Files panorama_fish_eye Note 3 lens  
Writing of Multiple Program Files panorama_fish_eye Note4 lens  
Writing of Unique Codes lens lens  
Selection of Multiple Emulators panorama_fish_eye Note5 lens When multiple emulators are connected to a single PC, they can be selected from the Renesas Flash Programmer.
Basic Writing Functions lens lens Blank check, erase, writing, verification, read-out, security setting, checksum, autoprocedure, setup and acquisition of flash options
Sequential Execution of Multiple Commands (for Erasure, Programming, Verification, etc.) lens lens  

lens= Available | panorama_fish_eye = Partly Available

Notes:

  1. By using the script execution function
  2. By using command-line options
  3. Only supported for RL78, 78K0, 78K0R, and V850 products
  4. Supported by connecting program files (only for RX and RH850 products)
  5. Supported for RX and RH850 products