Overview
Videos & Training
When you need MCU/MPU technical information, you can quickly find it on e² studio without surfing the web. This video demonstrates how to easily access MCU/MPU technical information using the Smart Browser.
Additional Details
Product Lineup
The product has five features for more efficient development.
| Smart Utility | IDE |
|---|---|
| Smart Configurator | CS+/e² studio |
| Smart Manual | CS+/e² studio |
| Smart Browser | CS+/e² studio |
| Assistant for Optimization | e² studio |
| Open-source Plugins | CS+ (partially)/e² studio |
Smart Configurator
The Smart Configurator is a utility for combining software as you wish. It supports the following three functions related to the embedding of Renesas drivers in your systems.
- Importing middleware in the form of FIT (Firmware Integration Technology) modules
- Generating driver code
- Setting pins
Smart Manual
Smart Manual makes it easy to find a hardware manual or information on the registers of a Renesas device (Note1).
The [Smart Manual] view is for browsing through hardware manuals and searching for occurrences of the names of registers (Note2) or keywords (Note3) in the manual.
The smart manual features also include popping up a description of the specifications in response to placing the mouse cursor over a register name or API function name (Note4) while editing.
Notes
- Some devices are not supported.
- Information on the registers and bits of peripheral I/O is searchable.
- Topical key words are used in searching for manuals.
- Output functions by a code generator (for RX, RL78, and RZ devices), FIT modules (for RX devices), and service calls to Renesas real-time OS (RI600V4).
Smart Browser
With the Smart Browser, you can easily find and display the latest Renesas hardware manuals, technical updates, and application notes from within the e² studio or CS+. It is also able to download sample code and import projects from projects which include sample code.
In CS+, searching for FAQs that match keywords you have entered is also possible.
Assistant for Optimization
The assistant for optimization assists in optimizing amounts of executable program code. This tool lets you easily see the changes in code size produced by changing compiler and linker options for building, so can help by shortening the time needed to reduce amounts of code.
Open-source Plugins that are Useful in Development
The e² studio also supports plugins which are useful for any development, such as for managing problems, version control, code reviews, and developing documentation. (Note1)
- Trac for managing bugs and requirements
- Subversion and Git for version and configuration control (Note2)
- AgileReview for code reviews
- Doxygen for developing documentation
- Jenkins for build management
- CUnit and Unity for testing
Note
- The above open-source tools can be found on their respective official download pages. Refer to the relevant page for the license conditions of each. Note that Renesas assumes no responsibility for failures of or other problems with this software.
- Those that can be run from a Windows Explorer window can also be run from the CS+ project tree (e.g. version management tools).
Support
Support Communities
- DA14531 Extended Sleep Mode
Hi Dialog, After putting My DA14531 into Extended sleep mode by setting static const sleep_state_t app_default_sleep_mode = ARCH_EXT_SLEEP_ON; in user_config.h file, How do i come to know whether my device is in extended sleep mode or not? And how to check ...
Mar 14, 2022 - SmartSnippetsToolbox Flash memory issues with DA1453x remote support pack
Dear team, I've come across what seems to be an abonrmal behavior of the flash memory utility within SmartSnippets Toolbox. I have a DA14531 USB development kit used as a programming probe through SWD interface with a custom board. The latter embeds a DA14531 interfaced with an external FLASH ...
Sep 28, 2021 - DA14531 Schematic review
... t want to use JTAG. I already have a USB-to-TTL dongle which I'd like to use for flashing the firmware through the SmartBond Flash Programmer utility. Firmware I intend to use is the CodeLess default firmware (set one) which I'll control through an external STM32U5 MCU ...
May 19, 2026
Knowledge Base
- Error (E0210002) occurs when connecting MCU and E1 (E2, E2 Lite, E1, E20)
Install the CS+ QE, which is necessary for debugging on the CS+ V4.00.00 or later.The CS+ supports Smart Utility and QE (Quick and Effective tool solution), which are advanced development environment tools. Download the suitable CS+ QE module for the CS+ which you are using. To download ...
Mar 8, 2021 - e² studio FAQs
... studio tutorial? Why e² studio Help tree's [+][-] buttons are not working? Where can I find detailed information on Subversive plugin and SVN? Errors about ‘Smart Manual Discovery’ are shown immediately after launching e² studio. ”Unable to download Smart Manual Catalog” Error When Starting e² studio Installing e² studio plugins ...
Jul 30, 2026 - RL78 Family: Creating Segment LCD drivers using Segment LCD QE tool and using them to display custom patterns
... and select the RL78L23_FastPrototypingBoard as the Target Board as well as select COM Port for creating Hardware Debug Configuration. Don't forget to add smart configurator. After project is created; open smart configurator window and add the LDC controller driver and configure properties such as bias mode, segment and ...
Jul 6, 2026