Overview
Description
The Renesas integrated development environment, or the High-performance Embedded Workshop, supports Tcl/Tk Version 8.4.4. Tcl/Tk is comprised of a class member "Tcl" of script language (Tool Command Language) and the "Tk" (Tool Kit) used to program a graphical user interface. Use of Tcl/Tk helps to create appropriate GUIs that suit the development environment, in addition to the functions and GUIs supplied by the High-performance Embedded Workshop, thereby extending the development environment further.
Target Devices
Documentation
|
|
|
---|---|---|
Type | Title | Date |
Release Note | PDF 307 KB 日本語 | |
Manual - Development Tools | PDF 4.16 MB 日本語 | |
Manual - Development Tools | PDF 1.85 MB 日本語 | |
Application Note | PDF 1.43 MB | |
4 items
|
Design & Development
Additional Details
Functions
The High-performance Embedded Workshop offers a Console window that supports Tcl/Tk programming and a GUI window.
Usage and a list of commands
The Console window of the High-performance Embedded Workshop permits Tcl/Tk programming to be performed in interpreter mode or script file load mode.
- Interpreter mode
- Tcl/Tk commands are executed by entering them directly in the Console window.
- Script file load mode
- A Tcl/Tk script file created beforehand is loaded and executed in the Console window.
During programming with Tcl/Tk, various commands supported in the High-performance Embedded Workshop environment can be used. By using Tcl/Tk and these commands in combination, it is possible to create GUIs that control the High-performance Embedded Workshop environment.
[Example of High-performance Embedded Workshop Usable in Tcl/Tk]
- Execution relevance
- Download relevance
- Register relevance
- Memory relevance
- Assemble/Disassemble relevance
- Break relevance
- Trace relevance
- Coverage relevance
- Performance measurement relevance
- Script/log file relevance
- Map relevance
- Simulation configuration relevance
- Standard I/O and file I/O relevance
- Utility relevance
- Projects and Workspace relevance
The usable commands of the High-performance Embedded Workshop differ with the target MCU for which the simulator and emulator are used. For details on how to use, refer to Tcl/Tk Application Notes.
Basic Sample Programs
Basic Tcl/Tk sample programs are supplied from Renesas. Use these samples to understand the basic method of programming.
- Tcl sample program
- This sample program uses the basic commands of Tcl. Download (Tcl sample program)
- Tk sample program
- This sample program uses the basic commands of Tk. Download (Tk sample program)