Mar. 26, 2024
This site provides information on the compatibility of Renesas Software with Microsoft Windows® 10.
Note that operation of products not shown in this site has not been confirmed, and there is no future plan to do so.
From version 8.07.00, integrated Development Environment CS+ has ended support Windows 32-bit version.
◎: | Product supported on Windows® 10 as the operating environment. |
◯: | There is no problem in the basic operations in Windows® 10. However, software has to be updated or related software has to be installed in some cases. Restrictions that do not significantly affect operation, such as some characters missing on display, are not indicated. Note that there is no plan to lift the restrictions in Windows® 10. |
- : | Confirmed basic operations with restrictions in Windows® 10 or Not operable. |
Cautions: | ・There may be more restrictions other than those shown in the site depending on environment in use. ・Please understand in advance that additions and changes to the information on the page may be made as required. |
Reference: | For the release schedules of our software tools compatible with other Windows, please refer to here. |
Table of Contents
- Development Environment of RZ Family
- Development Environment of RISC-V MCU
- Development Environment of RH850 Family
- Development Environment of RX Family
- Development Environment of RL78 Family
- Development Environment of SH Family
- Development Environment of V850 Family
- Development Environment of H8SX, H8S, H8 Family
- Development Environment of R8C and M16C Families
- Development Environment of 78K0R
- Development Environment of 78K0S
- Development Environment of 78K0
- Development Environment of other MCUs
- Related Tool News
Development Environment of RZ Family
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | e² studio | ◎ | ◎ | Supported by V4.1.0 | ||
Code Generator | AP4 for RZ | ◎ | ◎ | Supported by V1.01.00 |
Development Environment of RISC-V MCU
Classification | Product name | Additional information | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|
Integrated Development Environment | e² studio | ◎ | Supported by 2024-01.1 | ||
Programmer | Renesas Flash Programmer V3 | ◎ | Supported by V3.14.00 | ||
PG-FP6 | ◎ | Supported by V1.11.00 |
Development Environment of RH850 Family
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | CS+ | Including build and debugging tool | ◎ | ◎ | Supported by CS+ for CC V3.02.00 | |
RTOS | RI850V4 RH Real-time OS for RH850 Family | Supported by CS+ / GHS | ◎ | ◎ | Operation has been confirmed in V2.01.00 | |
Compiler | C Compiler Package for RH850 Family (CC-RH) | ◎ | ◎ | Supported by V1.03.00 | ||
Programmer | Renesas Flash Programmer V2 | ◯ | ◯ | Operation has been confirmed in V2.05.02 | Refer to related tool news No.9 | |
Renesas Flash Programmer V3 | ◎ | ◎ | Supported by V3.00.00 | Refer to related tool news No.9 | ||
PG-FP5 | ◎ | ◎ | Supported by GUI: V2.14 | No.9 |
Development Environment of RX Family
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | CS+ | Including build and debugging tool | ◎ | ◎ | Supported by CS+ for CC V3.02.00 | |
e² studio | ◎ | ◎ | Supported by V4.1.0 | |||
High-performance Embedded Workshop | Products including High-performance Embedded Workshop should be updated to the latest version. | ◯ | ◯ | Operation has been confirmed in V.4.09.01 | ||
└ Install Manager | ◯ | ◯ | Operation has been confirmed in V.1.04.00 | |||
└ Auto Update Utility | ◯ | ◯ | Operation has been confirmed in V.1.05.00 | |||
Code Generator | AP4 for RX | ◎ | ◎ | Supported by V1.07.00 | ||
Peripheral Driver Generator | ◎ | ◎ | Operation has been confirmed in V2.09 | |||
RTOS | Real-time OS for RX600 Series [RI600V4] | Supported by CS+ | ◎ | ◎ | Operation has been confirmed in V1.04.00 | |
Real-time OS for RX600, RX200 Series [RI600PX] | Supported by CS+ | ◎ | ◎ | Operation has been confirmed in V1.02.00 | ||
Real-time OS for RX600, RX200 Series [RI600/4] | Supported by High-performance Embedded Workshop | ◯ | ◯ | Operation has been confirmed in V.1.01 R01 | ||
Real-time OS for RX600 Series [RI600/PX] | Supported by High-performance Embedded Workshop | ◯ | ◯ | Operation has been confirmed in V.1.00 R01 | ||
Compiler | C/C++ Compiler Package for RX Family | without IDE | ◎ | ◎ | Supported by V2.04.00 | |
Supported by CS+ | ◎ | ◎ | Supported by V2.04.00 | |||
Supported by High-performance Embedded Workshop | ◯ | ◯ | Operation has been confirmed in V.1.02 R01 | |||
Simulator | Simulator Debugger for RX Family | Included in a compiler package with High-performance Embedded Workshop | ◯ | ◯ | Operation has been confirmed in V.1.02.01 | |
Emulator | E1/E20 Emulator Software | High-performance Embedded Workshop is included | ◯ | ◯ | Supported by V.1.03 R00 Acquire the USB Driver here. | Refer to related tool news No.9, No.13, No.17 |
└ External Flash Definition Editor | ◯ | ◯ | Supported by V.1.00 R01 | |||
RX E100 Emulator Software | High-performance Embedded Workshop is included | ◯ | ◯ | Operation has been confirmed in V.1.00 R00 Acquire the USB Driver here. | No.14 | |
Programmer | Renesas Flash Programmer V2 | ◯ | ◯ | Operation has been confirmed in V2.05.02 | Refer to related tool news No.9 | |
Renesas Flash Programmer V3 | ◎ | ◎ | Supported by V3.00.00 | Refer to related tool news No.9 | ||
Flash Development Toolkit | ◎ | ◎ | Supported by V.4.09 R03 | No.9 | ||
PG-FP5 | ◎ | ◎ | Supported by GUI: V2.14 | No.9 |
Development Environment of RL78 Family
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | CS+ | Including build and debugging tool | ◎ | ◎ | Supported by CS+ for CC V3.02.00 and CS+ for CA,CX V3.01.00 | |
e² studio | ◎ | ◎ | Supported by V4.1.0 | |||
Code Generator | AP4 for RL78 | ◎ | ◎ | Operation has been confirmed in V1.09.00 | ||
Applilet3 for RL78 | ◎ | ◎ | Operation has been confirmed in V1.09.00 | |||
RTOS | Real-time OS for RL78 family and 78K0R [RI78V4] | Supported by CS+ | ◎ | ◎ | Operation has been confirmed in V1.00.02 | |
Real-time OS for RL78 family [RI78V4] | Supported by CS+ | ◎ | ◎ | Operation has been confirmed in V2.00.00 | ||
Compiler | C/C++ Compiler Package for RL78 Family | without IDE | ◎ | ◎ | Supported by V1.02.00 | |
Supported by CS+ | ◎ | ◎ | Supported by V1.02.00 | |||
Programmer | Renesas Flash Programmer V2 | ◯ | ◯ | Operation has been confirmed in V2.05.02 | Refer to related tool news No.9 | |
Renesas Flash Programmer V3 | ◎ | ◎ | Supported by V3.00.00 | Refer to related tool news No.9 | ||
PG-FP5 | ◎ | ◎ | Supported by GUI: V2.14 | No.9 |
Development Environment of SH Family
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | High-performance Embedded Workshop | Products including High-performance Embedded Workshop should be updated to the latest version. | ◯ | ◯ | Operation has been confirmed in V.4.09.01 | |
└ Install Manager | ◯ | ◯ | Operation has been confirmed in V.1.04.00 | |||
└ Auto Update Utility | ◯ | ◯ | Operation has been confirmed in V.1.05.00 | |||
Code Generator | Peripheral Driver Generator | ◯ | ◯ | Operation has been confirmed in V.1.04 | ||
RTOS | Real-time OS for SH-4 and SH-4A [HI7750/4] | ◯ | ◯ | Operation has been confirmed in V.2.03 R00 | Help function is disabled. | |
Real-time OS for SH-3, SH3-DSP and SH4AL-DSP [HI7700/4] | ◯ | ◯ | Operation has been confirmed in V.2.04 R00 | Help function is disabled. | ||
Real-time OS for SH2A-DUAL [HI7200/MP] | ◯ | ◯ | Operation has been confirmed in V.1.01 R00 | Help function is disabled. | ||
Real-time OS for SH-1, SH-2, SH2-DSP, SH-2A and SH2A-FPU [HI7000/4] | ◯ | ◯ | Operation has been confirmed in V.2.03 R01 | Help function is disabled. | ||
μITRON4.0/PX Specification Real-time OS for SH4AL-DSP and SH-4A [HI7300/PX] | ◯ | ◯ | Operation has been confirmed in V.1.03 R00 | Help function is disabled. | ||
Compiler | C/C++ Compiler Package for SuperH Family | High-performance Embedded Workshop is included | ◯ | ◯ | Operation has been confirmed in V.9.04 R02 | |
MISRA C Rule Checker SQMlint | ◯ | ◯ | Operation has been confirmed in V.1.03 R00B | |||
Simulator | Simulator debugger for the SuperH RISC engine family | Included in a compiler package with High-performance Embedded Workshop | ◯ | ◯ | Operation has been confirmed in V.9.10.01 | |
Emulator | HS0005KCU01H and HS0005KCU02H E10A-USB | Emulator Software | ◯ | ◯ | Operation has been confirmed in V.3.05 It will be compatible by installing E10A-USB Emulator Software V.3.05 Release 00 (Full package). Note: Emulator Software for device group does not include Windows® 10 compatible driver. Acquire the USB Driver here. | Refer to related tool news No.9 |
License Tool for Device Group Additions | ◯ | ◯ | Operation has been confirmed in V.5.00 R00 Note: Alternatively, it will be compatible by installing E10A-USB Emulator Software V.3.05 Release 00 (Full package). | |||
E10A-USB for SuperH RISC engine family of multi-core MCUs HS0005KCU04H, HS0005KCU14H | Emulator Software | ◯ | ◯ | Operation has been confirmed in V.2.02 R00 Acquire the USB Driver here. | ||
E200F | - | - | No plan to support | |||
E6000H | - | - | No plan to support | |||
Programmer | Flash Development Toolkit | Combination with COM | ◎ | ◎ | Supported by V.4.09 R03 | No.9 |
Combination with E8a | ◯ | ◯ | Operation has been confirmed in V.4.09 R03 | No.9 | ||
PG-FP5 | ◎ | ◎ | Supported by GUI: V2.14 | No.9 |
Development Environment of V850 Family
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | CS+ | Including build and debugging tool | ◎ | ◎ | Supported by CS+ for CA,CX V3.01.00 | |
QS850 (CubeSuite) | ◯ | ◯ | Operation has been confirmed in V1.40 | No.7, No.8, No.10 | ||
PM+ | Including CA703000 (CA850) | ◯ | - | Operation has been confirmed in V6.32 with the restrictions listed in the right column. Note: Updating device file installer to V.3.30 is required. See the restrictions on the right when using V3.30. | No.1, No.2, No.4 | |
Code Generator | Applilet2 for V850ES/Fx3 | ◯ | ◯ | Operation has been confirmed in V2.43 | No.12 | |
Applilet2 for V850ES/Sx3 | ◯ | ◯ | Operation has been confirmed in V2.41 | No.12 | ||
Applilet3 for V850 | ◎ | ◎ | Supported by V1.01.00 | |||
RTOS | Real-time OS for V850 [RI850V4] | Supported by CS+ | ◎ | ◎ | Operation has been confirmed in V1.01.00 | |
Real-time OS for V850 [RI850MP] | Supported by CS+ | ◎ | ◎ | Operation has been confirmed in V1.00.01 | ||
Real-time OS for V850 [RX850V4] | Supported by CubeSuite V1.40 | ◯ | ◯ | Operation has been confirmed in V4.30 | Installation of .NET3.5 is necessary. | |
Compiler | CA703000 (CA850) | ◯ | - | Operation has been confirmed in V3.44 or later with the restrictions listed in the right column. | No.1, No.2, No.3, No.4 | |
Simulator | SM703000 (SM850) | ◯ | - | Operation has been confirmed in V3.00 or later with the restrictions listed in the right column. | No.1, No.2, No.5 | |
SM703100 (SM+ for V850) | ◯ | - | Operation has been confirmed in V2.00 or later with the restrictions listed in the right column. | No.1, No.2, No.5, No.6, No.11 | ||
SM703239-B (SM+ for V850ES/Fx2) | ◯ | - | Operation has been confirmed in V2.22 or later with the restrictions listed in the right column. | No.1, No.2, No.5, No.6 | ||
SM703385-B (SM+ for V850ES/Fx3) | ◯ | - | Operation has been confirmed in V2.43 or later with the restrictions listed in the right column. | No.1, No.2, No.5 | ||
Emulator | ID703000 (ID850) | - | - | |||
ID703000-QB (ID850QB) | ◯ | - | Operation has been confirmed in V3.61 or later with the restrictions listed in the right column. | Refer to related tool news No.1, No.2, No.5, No.8, No.9 | ||
Programmer | Renesas Flash Programmer V2 | ◯ | ◯ | Operation has been confirmed in V2.05.02 | Refer to related tool news No.9 | |
PG-FP5 | ◎ | ◎ | Supported by GUI: V2.14 | No.9 |
Development Environment of H8SX, H8S, H8 Family
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | High-performance Embedded Workshop | Products including High-performance Embedded Workshop should be updated to the latest version. | ◯ | ◯ | Operation has been confirmed in V.4.09.01 | |
└ Install Manager | ◯ | ◯ | Operation has been confirmed in V.1.04.00 | |||
└ Auto Update Utility | ◯ | ◯ | Operation has been confirmed in V.1.05.00 | |||
Code Generator | Peripheral Driver Generator | ◯ | ◯ | Operation has been confirmed in V.1.04 | ||
RTOS | Real-time OS for H8SX, H8S Family [HI1000/4] | ◯ | ◯ | Operation has been confirmed in V.1.06 R00 | Help function is disabled. | |
Compiler | C/C++ Compiler Package for H8SX, H8S, H8 Family | High-performance Embedded Workshop is included | ◯ | ◯ | Operation has been confirmed in V.7.00 R00 | |
MISRA C Rule Checker SQMlint | ◯ | ◯ | Operation has been confirmed in V.1.03 R00B | |||
Simulator | Simulator Debugger for the H8, H8S, H8SX family | Included in a compiler package with High-performance Embedded Workshop | ◯ | ◯ | Operation has been confirmed in V.5.09.00 | |
Emulator | E8a | Emulator Software | ◯ | ◯ | Operation has been confirmed in V.1.05 R00 | Refer to related tool news |
HS0005KCU01H and HS0005KCU02H E10A-USB | Emulator Software | ◯ | ◯ | Operation has been confirmed in V.3.05 It will be compatible by installing E10A-USB Emulator Software V.3.05 Release 00 (Full package). Note: Emulator Software for device group does not include Windows® 10 compatible driver. Acquire the USB Driver here. | No.9 | |
License Tool for Device Group Additions | ◯ | ◯ | Operation has been confirmed in V.5.00 R00 Note: Alternatively, it will be compatible by installing E10A-USB Emulator Software V.3.05 Release 00 (Full package). | |||
E10T-USB | - | - | ||||
H8SX E100 | Emulator Software | ◯ | ◯ | Operation has been confirmed in V.1.01 R00 Acquire the USB Driver here. | Refer to related tool news No.9, No.13 | |
H8S/Tiny, H8S/2400 E100 | Emulator Software | ◯ | ◯ | Operation has been confirmed in V.2.00 R00 Acquire the USB Driver here. | No.14 | |
E6000H | - | - | Not confirmed. | |||
E6000 | - | - | Not confirmed. | |||
Programmer | Flash Development Toolkit | Combination with COM | ◎ | ◎ | Supported by V.4.09 R03 | No.9 |
Combination with E8a | ◯ | ◯ | Operation has been confirmed in V.4.09 R03 | No.9 |
Development Environment of R8C and M16C Families
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | High-performance Embedded Workshop | Products including High-performance Embedded Workshop should be updated to the latest version. | ◯ | ◯ | Operation has been confirmed in V.4.09.01 | |
└ Install Manager | ◯ | ◯ | Operation has been confirmed in V.1.04.00 | No.15 | ||
└ Auto Update Utility | ◯ | ◯ | Operation has been confirmed in V.1.05.00 | |||
Code Generator | Peripheral Driver Generator | ◯ | ◯ | Operation has been confirmed in V.1.04 | ||
RTOS | Real-time OS for M16C Series and R8C Family [M3T-MR30/4] | ◯ | ◯ | Operation has been confirmed in V.4.01 R00 Note: When any build is performed, use your compiler package V.5.45 R01 or later. | ||
Real-time OS for R8C Family [MR8C/4] | ◯ | ◯ | Operation has been confirmed in V.1.01 R00 Note: When any build is performed, use your compiler package V.5.45 R01 or later. | |||
Real-time OS for R32C/100 Series [M3T-MR100/4] | ◯ | ◯ | Operation has been confirmed in V.1.01 R00. Note: When any build is performed, use your compiler package V.5.45 R01 or later. | |||
Compiler | C/C++ Compiler Package for R8C and M16C Families | Note : This product contains the following three compilers. High-performance Embedded Workshop is included | ◯ | ◯ | ||
└ C/C++ Compiler Package for M16C Series and R8C Family [M3TNC30WA] | ◯ | ◯ | Operation has been confirmed in V.5.45 R01 and V6.00.00 | |||
└ C Compiler Package for R32C Series | ◯ | ◯ | Operation has been confirmed in V.1.02.01 | |||
└ C Compiler Package for M32C Series [M3TNC308WA] | ◯ | ◯ | Operation has been confirmed in V.5.42.00 | |||
MISRA C Rule Checker SQMlint | ◯ | ◯ | Operation has been confirmed in V.1.03 R00B | |||
Simulator | Simulator Debugger for M16C Series and R8C Family | Included in a compiler package with High-performance Embedded Workshop | ◯ | ◯ | Operation has been confirmed in V.1.05 R00 | |
Emulator | E1/E20 R8C | Emulator Debugger | ◯ | ◯ | Operation has been confirmed in V.1.00.00 Acquire the USB Driver here. | Refer to related tool news No.9 |
E8a | Emulator Software | ◯ | ◯ | Operation has been confirmed in V.1.05 R00 | No.13 | |
R32C/100 E30A | Emulator Debugger | ◯ | ◯ | Operation has been confirmed in V.1.02 R00 Acquire the USB Driver here. | No.14 | |
M16C R8C E100 | Emulator Software | ◯ | ◯ | Operation has been confirmed in V.1.03 R00 Acquire the USB Driver here. | ||
PC7501 | - | - | Refer to the FAQ for Windows® 7:FAQ 1010194 | |||
Compact Emulators | - | - | ||||
External Flash Definition Editor | ◯ | ◯ | Supported by V.1.00 R01 | Refer to related tool news No.9, No.13, No.14 | ||
Programmer | Flash Development Toolkit | Combination with COM, E1, E20 | ◎ | ◎ | Supported by V.4.09 R03. | No.9 |
Combination with E8a | ◯ | ◯ | Operation has been confirmed in V.4.09 R03 | No.9 | ||
PG-FP5 | ◎ | ◎ | Supported by GUI: V2.14 | No.9 |
Development Environment of 78K0R
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | CS+ | Including build and debugging tool | ◎ | ◎ | Supported by CS+ for CA,CX V3.01.00 | |
QS78K (CubeSuite) | ◯ | ◯ | Operation has been confirmed in V1.40 | No.7, No.8, No.10 | ||
PM+ | Note: Including RA78K0R | ◯ | - | Operation has been confirmed in V6.32 with the restrictions listed in the right column. Note: Updating device file installer to V.3.30 is required. See the restrictions on the right when using V3.30. | No.1, No.2, No.4 | |
Code Generator | Applilet3 for 78K | ◎ | ◎ | Operation has been confirmed in V1.02.00 | ||
RTOS | Real-time OS for RL78 family and 78K0R [RI78V4] | Supported by CS+ | ◎ | ◎ | Operation has been confirmed in V1.00.02 | |
Real-time OS for 78K0R [RX78K0R] | Supported by CubeSuite V1.40 | ◯ | ◯ | Operation has been confirmed in V4.30 | Installation of .NET3.5 is necessary. | |
Compiler | CC78K0R | ◯ | - | Operation has been confirmed in V2.13 or later with the restrictions listed in the right column. | No.1, No.2 | |
RA78K0R | Assembler | ◯ | - | Operation has been confirmed in V1.33 or later with the restrictions listed in the right column. | No.1, No.2, No.4 | |
Simulator | SM781000 (SM+ for 78K0R) | ◯ | - | Operation has been confirmed in V2.41 or later with the restrictions listed in the right column. | No.1, No.2, No.5 | |
SM781188-B (SM+ for 78K0R/Kx3) | ◯ | - | Operation has been confirmed in V2.41 or later with the restrictions listed in the right column. | No.1, No.2, No.5 | ||
Emulator | ID78K0R-QB | Software for MINICUBE2 and IECUBE | ◯ | - | Operation has been confirmed in V3.61 or later with the restrictions listed in the right column. | Refer to related tool news No.1, No.2, No.5, No.8, No.9 |
Programmer | Renesas Flash Programmer V2 | ◯ | ◯ | Operation has been confirmed in V2.05.02 | Refer to related tool news No.9 | |
PG-FP5 | ◎ | ◎ | Supported by GUI: V2.14 | No.9 |
Development Environment of 78K0S
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | PM+ | Note: Including RA78K0S | ◯ | - | Operation has been confirmed in V6.32 with the restrictions listed in the right column. Note: Updating device file installer to V.3.30 is required. See the restrictions on the right when using V3.30. | No.1, No.2, No.4 |
Code Generator | Applilet2 for 78K0S/Kx1+ | ◯ | ◯ | Operation has been confirmed in V2.41 | No.12 | |
Compiler | CC78K0S | ◯ | - | Operation has been confirmed in V2.01 or later with the restrictions listed in the right column. | No.1, No.2 | |
RA78K0S | Assembler | ◯ | - | Operation has been confirmed in V2.00 or later with the restrictions listed in the right column. | No.1, No.2, No.4 | |
Simulator | SM78K0S | ◯ | - | Operation has been confirmed in V3.00 or later with the restrictions listed in the right column. | No.1, No.2, No.5 | |
SM789000 (SM+ for 78K0S) | ◯ | - | Operation has been confirmed in V2.42 or later with the restrictions listed in the right column. | No.1, No.2, No.5 | ||
Emulator | ID78K0S-NS | - | - | |||
ID78K0S-QB | ◯ | - | Operation has been confirmed in V3.01 or later with the restrictions listed in the right column. | Refer to related tool news No.1, No.2, No.5, No.8, No.9 | ||
Programmer | PG-FP5 | ◎ | ◎ | Supported by GUI: V2.14 | No.9 |
Development Environment of 78K0
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Integrated Development Environment | CS+ | Including build and debugging tool | ◎ | ◎ | Supported by CS+ for CA,CX V3.01.00 | |
QS78K (CubeSuite) | ◯ | - | Operation has been confirmed in V1.40 | No.7, No.8, No.10 | ||
PM+ | Note: Including RA78K0 | ◯ | - | Operation has been confirmed in V6.32 with the restrictions listed in the right column. Note: Updating device file installer to V.3.30 is required. See the restrictions on the right when using V3.30. | No.1, No.2, No.4 | |
Code Generator | Applilet3 for 78K | ◎ | ◎ | Operation has been confirmed in V1.02.00 | ||
Applilet2 for 78K0/Fx2 | ◯ | ◯ | Operation has been confirmed in V2.42 | No.12 | ||
Applilet2 for 78K0/Kx2 | ◯ | ◯ | Operation has been confirmed in V2.42 | No.12 | ||
Applilet2 for 78K0/Lx2 | ◯ | ◯ | Operation has been confirmed in V2.41 | No.12 | ||
Applilet2 for 78K0/Lx3 | ◯ | ◯ | Operation has been confirmed in V2.41 | No.12 | ||
Compiler | CC78K0 | ◯ | - | Operation is available in V4.00 or later with the restrictions listed in the right column. | No.1, No.2 | |
RA78K0 | Assembler | ◯ | - | Operation is available in V4.01 or later with the restrictions listed in the right column. | No.1, No.2, No.4 | |
Simulator | SM78K0 | ◯ | - | Operation is available in V3.00 or later with the restrictions listed in the right column. | No.1, No.2, No.5 | |
SM780000 (SM+ for 78K0) | ◯ | - | Operation is available in V2.20 or later with the restrictions listed in the right column. | No.1, No.2, No.5, No.6 | ||
Emulator | ID78K0-NS | - | - | |||
ID78K0-QB | ◯ | - | Operation is available in V3.21 or later with the restrictions listed in the right column. | Refer to related tool news No.1, No.2, No.5, No.8, No.9 | ||
Programmer | Renesas Flash Programmer V2 | ◯ | ◯ | Operation has been confirmed in V2.05.02 | Refer to related tool news No.9 | |
PG-FP5 | ◎ | ◎ | Supported by GUI: V2.14 | No.9 |
Development Environment of other MCUs
Classification | Product name | Additional information | 32-bit | 64-bit | Status for Windows® 10 | Restrictions |
---|---|---|---|---|---|---|
Tools for Smart Analog | SA-Designer | ◯ | ◯ | Operation has been confirmed in V1.0.3.00 | ||
RTOS | CS+ Partner OS Aware Debugging Plug-in | ◯ | ◯ | Supported by V3.01.00 | ||
e² studio Partner OS Aware Debugging | ◯ | ◯ | Supported by e² studio V4.0 | |||
High-performance Embedded Workshop Real-Time OS Aware Debugging | ◯ | ◯ | Supported by High-performance Embedded Workshop V4.09 | |||
High-performance Embedded Workshop Real-Time OS Aware Debugging Extension | ◯ | ◯ | Supported by V.1.08 R00 | Help function is disabled. | ||
Compiler | C/C++ Compiler Package for M32R Family | High-performance Embedded Workshop is included High-performance Embedded Workshop should be updated to the latest version. | ◯ | ◯ | Operation has been confirmed in V.5.01 R01 |
Related Tool News
Note that the following tool news are applicable to Windows® 10.
- Note on Using Renesas-Made Emulators
--Problem with Using Emulators Connected to Windows 7-Installed PCs--
https://www.renesas.com/document/tnn/note-using-renesas-made-emulators-problem-using-emulators-connected-Windows-7-installed-pcs