Skip to main content

China RoHS

China's Administrative Measures for Restrictions on the Use of Hazardous Substances in Electrical and Electronic Products, also known as Amendment China RoHS, requires an indication of the hazardous substance used and the product Environment Friendly Use Period (EFUP) for end products that the product Environment Friendly Use Period (EFUP) for end products that contain specified toxic and hazardous substances. Semiconductor products are not electrical and electronic end products, so information related toare not electrical and electronic end products, and product Environment Friendly Use Period (EFUP) values is provided through sales companies and authorized dealers without directly marking the products. (officially announced January 21, 2016/ enforced July 1, 2016)

Substances Restricted by the China RoHS and its Maximum Concentration Value

Substances restricted by the China RoHS Maximum concentration value (ppm)
Lead (Pb) 1,000
Mercury (Hg) 1,000
Cadmium (Cd) 100
Hexavalent chromium (Cr6+) 1,000
Polybrominated biphenyls (PBB) 1,000
Polybrominated diphenyl ethers (PBDE) 1,000