Renesas packing is designed to protect semiconductors during transit and development.
Packing Types
Renesas Electronics has three packing types.
Magazine | Tray | Tape | |
---|---|---|---|
Packing Container | ![]() |
![]() |
![]() |
Packing Box | ![]() |
![]() |
![]() |
Packaging Label
The inner label example shown below applies to all products shipped since January 2012.
Example Label
Brevity code | Description | |
---|---|---|
① | SPN | Booking parts number |
② | PN | Customer parts number |
③ | QTY | Quantity |
④ | T・L・B | Mounting condition(In special case) |
⑤ | MSL | Moisture sensitivity levels (In special case) |
(4) and (5) listed above are not labeled on all products. See elements for special conditions for details.
Handling Guide
Important! Users must read and understand the Handling Guide before opening semiconductor packing containers. Failure to properly handle the packing container increases the risk of system assembly defects and / or serious quality & reliability problems.
Guarding Against Static Electricity
Guarding against static electricity means first of all stopping it from occurring, and then if it does, discharging it appropriately (rapid discharge of a semiconductor device may damage the device).
For this reason, it is important to curb friction-charged static electricity caused by vibration during transportation, and to ensure an appropriate environment for handling of semiconductor devices is maintained. The operator handling semiconductor devices must have appropriate knowledge about static electricity.
The following table outlines measures to take when packing semiconductor devices, as well as examples of general precautions.
Packing Type | Guarding Against Static Electricity |
---|---|
Magazine | Antistatic additive is applied to the surface of plastic magazines, except for magazines made of aluminum or plastic material milled with carbon. Electrically conductive trays (plastic material milled with carbon) are used. |
Tray | Electrically conductive trays (plastic material milled with carbon) are used.。 |
Moisture Barrier Bag | Aluminum laminate bags with static electricity diffusion are used, |
Tape | Emboss taped products use static electricity diffusion carrier tapes and reels. |
Re-Use / Recycling of Packing Container
Renesas is committed to preserving the environment. Please recycle the packing containers (e.g., trays), or send back to Renesas Electronics for reuse.