This session spotlights a powerful, easy-to-use tool for developing Graphical User Interfaces (GUIs) for LCD-equipped embedded systems that employ Renesas' RZ processors. We will present, in a step-by-step fashion, two methods to create and optimize attractive and functional GUIs. One approach uses Express Logic's GUIX™ small-footprint, low-overhead runtime engine and development tool and is implemented via simple C-callable services. The other approach applies the capabilities of the GUIX Studio, a PC-based WYSIWYG companion tool for GUI creation. Both methods allow programmers and nonprogrammers alike to produce outstanding GUIs.
Jun 22, 2018