Skip to main content

FreeRTOS PubSub Demo with Trusted Secure IP (TSIP) - CK-RX65N V2 Setup 1 (1/4)

2024-10-09

This video provides a step-by-step guide on configuring the environment for the FreeRTOS PubSub demo with Trusted Secure ID (TSIP). It covers preparation, setting up AWS, and getting ready to run the demo project.

Related Resources

Renesas Key Wrap service - References from 1:37 to 1:55 in the video are as follows:

AWS SETUP - References from 2:27 to 2:38 in the video are as follows:

Preparing for the Demo Project - References from 2:43 to 2:55 in the video are as follows:
Reference the video for the project name, FreeRTOS version, and application.

Watch the rest of the video series below