Skip to main content

Getting Started with R-Car S4 Whitebox SDK on R-Car S4 Starter Kit

Jan 22, 2024

This video shows how to start up R-Car S4 Whitebox SDK with the R-Car S4 Starter Kit.

00:00 Opening
00:51 Set up the build environment
03:45 Build the image for R-Car S4 Starter Kit
05:56 Prepare host environment
06:44 Download firmware to the target board
08:14 Configure U-Boot and write images
10:34 Boot and confirm the operation