Skip to main content

How to set up and use TraceX® in a Renesas Synergy™ project using IAR Embedded Workbench

2018-06-22

The Renesas Synergy™ Platform includes TraceX®, which provides a graphical view of application and system activity over time. Like all of Synergy, TraceX is tightly integrated with the rest of the Synergy Platform and is easy to setup and use. In this video, you will see just how easy it is to setup TraceX on the Renesas Synergy Platform. You can download TraceX for Synergy from the Synergy Gallery.

Transcript

Optional Transcript goes here if available. Read through the transcript text and link any appropriate keywords and products that have pages.

Example:

There are many 12V rails in industrial applications today that need a buck converter to step the voltage down to a lower voltage and deliver up to 14 amps. The ISL85009, ISL85012 and ISL85014 are pin compatible, very efficient and are able to deliver up to 14 amps.