This demonstration shows motor control and fault detection with a Renesas MCU. The e-AI unit detects an abnormality with the motor installation from the acceleration sensor. In addition to the acceleration sensor, malfunction detection is also possible by using information stored in the motor control MCU, such as current, torque and rotation speed. e-AI makes motor control more intelligent, predicts the maintenance schedule, identifies the location of the failure, and realizes the endpoint in real time.
Jan 22, 2019