Skip to main content

QE for Capacitive Touch[RA] Tutorial: Use QE for Capacitive Touch with FSP in Keil® MDK

Sep 27, 2022

This video demonstrates how to use QE for Capacitive Touch with FSP in Keil® MDK for the RA2L1 capacitive Touch Evaluation system. 

0:00:00 Introduction
0:00:22 Generate files using QE for Capacitive Touch in e2 studio
0:01:12 Create the Capacitive Touch project for Keil® MDK
0:02:19 Add Touch drivers to the project in Keil® MDK
0:03:20 Copy QE files to Keil® MDK and build the project

Related resources: