Skip to main content

Renesas Radar Solution RH850/V1R-M

Jun 22, 2018

RH850/V1R-M is a 32-bit single-chip microcontroller with multiple CPUs, Code Flash, Data Flash, RAM, DMA controllers, many communication interfaces that are used in the automotive applications, A/D converters, timer units, etc. For the Radar function it incorporates a DSP toolkit with additional RAM and has a high speed differential interface. This chip is compliant with the functional safety standard required in the automotive applications (ISO26262).