Skip to main content

RZ/T RZ/N FSP Tutorial - Pin Configuration Function

2023-12-20

This video shows you how to use the FSP - Pin Configuration function for RZ/T and RZ/N devices. It teaches you how to set up pins using the Pins tab and shows examples of pin conflicts. It also shows what the pin setup looks like when it’s done, so you can check your work.

00:29 Introduction of Pin Configuration
04:36 Features Available in Pin Configuration GUI
07:28 Pin Conflict Example
11:57 Pin Configuration Output and Usage

FSP links

Board links