TOKYO, Japan ― Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today introduced the third generation DDR5 registered clock driver (RCD) as well as the first-generation client clock driver (CKD) for emerging DDR5 DRAM servers and client systems. With these new driver ICs, Renesas continues to be the only provider to offer a complete portfolio of DDR5 memory interfaces for dual inline memory modules (DIMMs), motherboards and embedded applications.
The DDR5 RCD and DDR5 CKD ICs enable the next generation of DIMMs with speeds of up to 6400 and 7200 megatransfers per second (MT/s), respectively, an increase from today’s 5600 MT/s transfer speeds. Renesas’ Gen 3 DDR5 RCD is designed for registered DIMMs (RDIMMs). The CKD supports speeds up to 7200 MT/s and is the first in the industry to interface with small-outline DIMMs (SODIMMs), unbuffered DIMMs (UDIMMs), high-performance gaming DIMMs and memory down applications for client platforms.
“As the industry’s leading provider of memory interface products, Renesas continues to make outstanding contributions in pushing the memory eco-system to new frontiers of performance and power” said Balaji Kanigicherla, Corporate Vice President and General Manager of the Advanced Mixed Signal and ASIC Solutions Division at Renesas. “By playing an integral role in defining and implementing DDR5 interface specifications, Renesas continues to be an important partner for the world’s leading SOC and DRAM players for DIMM and system-level bring up.”
“Intel® Xeon®-based platforms are designed to support memory intensive usages like predictive analytics that use deep learning and machine learning. Gen 3 RCD is a major milestone for the memory industry to help meet the bandwidth and scaling capacity needs of our datacenter customers”, said Dr. Dimitrios Ziakas, Vice President of Memory and IO Technologies at Intel. “The client clock driver is a new industry initiative to further enhance the client DIMM. Renesas and Intel have been collaborating with the industry to help ensure specification and implementations of the Gen 3 RCD and client clock driver to meet the market needs.”
The RCD driver buffers the command address (CA) bus, chip selects and clock between the host controller and DRAM modules, in addition to creating a BCOM bus to control LRDIMM data buffering. The new driver enhances decision-feedback equalizer (DFE) support by increasing the DFE taps from four to six to improve receiver margin, while I2C and I3C sideband bus support provides direct contact to the register access control.
The CKD buffers the clock between the host controller and DRAM, which is a new requirement for DDR5 DIMMs operating at speeds of up to 7200 MT/s for client DIMMs and memory down applications. The new clock driver supports I2C and I3C sideband access to enable asynchronous control and provides access to internal control words for configuring device features and adapting to different SODIMM and UDIMM configurations and memory down system applications.
RCD and CKD Driver Winning Combinations
Renesas has combined the RCD and CKD drivers with other compatible devices from its Winning Combinations portfolio, including DDR5 power management integrated circuits (PMICs) and serial presence detect (SPD) hubs for the CKD. The RCD can also be paired with Renesas’ temperature sensors, SPD Hub, PMICs, and data buffers. Winning Combinations are technically vetted system architectures from mutually compatible devices that work together seamlessly to bring an optimized, low-risk design for faster time to market. Renesas offers more than 400 Winning Combinations with a wide range of products from the Renesas portfolio to enable customers to speed up the design process and bring their products to market more quickly.
Availability
The RG5C172B0C0GBX#BC0 and RG5C172B0C0GBX#HC0 client clock drivers are sampling now in a 2.3mm x 5.8mm 35-FCBGA package and will be available in volume in the second half of 2023. The RG5R364A0C0GBY#BC0 and RG5R364A0C0GBY#HC0 DDR5 third-generation registered clock drivers are sampling now in an 8.7mm x 13.5mm FCCSP package and will be available in volume in the first half of 2024. More information on the new driver ICs is available at www.renesas.com/DDR5.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. The leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube, and Instagram.
(Remarks) Intel, the Intel logo, and other Intel marks are trademarks of Intel Corporation or its subsidiaries. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.