Skip to main content

Renesas Introduces Second-Generation of ClockMatrix Family of Network Synchronizers and Jitter Attenuators for Optical and Wireline Networks

New ClockMatrix 2 Delivers Industry’s First Single Chip Network Synchronizer and Jitter Attenuator with Ultra-Low Jitter Clock Outputs While Supporting all IEEE1588 operating modes

December 15, 2021

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced the ClockMatrix 2 high-performance, precision, multi-channel timing devices for 400/800Gbps optical transport and wireline network applications. Building on the ClockMatrix devices introduced in 2019 for 5G wireless and 100/200Gbps wireline network applications, the second-generation family delivers improved performance with phase jitter as low as 88fs-rms.

The highly integrated devices provide all the functionality needed to implement an IEEE1588 clock solution with jitter attenuation capabilities resulting in ultra-low jitter clock outputs for Synchronous Ethernet PHYs with data rates up to 112Gbps PAM-4, reducing design complexity and bill of materials (BOM) requirements, while also allowing customers to apply the timing devices to a wide variety of network applications.

“The shift to 5G is pushing the limits of network speed and precision, raising the bar on clock jitter and synchronization capabilities,” said Bobby Matinpour, Vice President of the Timing Products Division at Renesas. “The new ClockMatrix 2 family delivers on all fronts, with low jitter, high precision, and a wide range of synchronization features in a highly integrated single-chip solution.”

Key Features of the ClockMatrix 2 Family

  • Highly integrated, 6-channel precision timing source that eliminates the need for additional jitter attenuators for high-speed interfaces
  • 88fs-rms phase jitter on clock outputs to support ultra-low jitter clock outputs for high-speed serial links (up to 112Gbps PAM-4 PHYs)
  • Supports multiple standards and protocols including synchronous Ethernet (Sync-E), and IEEE1588
  • Adherence to G.8262.1 and G.8262 telecom boundary clock requirements and G.8273.2 Class C and Class D time accuracy

The ClockMatrix 2 system synchronizer can be combined with Renesas’ complementary analog and power offerings to create comprehensive solutions for a variety of applications. For example, ClockMatrix 2 is integrated into the 200/400/800Gbps Fixed Form Factor Switch Solution Winning Combination, along with analog and power offerings from Renesas. Renesas offers more than 250 Winning Combinations with compatible devices for a wide range of applications and end products. They can be found at www.renesas.com/win.

Availability

The RC32614A ClockMatrix 2 system synchronizer is available now. For more information, please visit https://www.renesas.com/clockmatrix. Optional PTP Clock Manager software is also available free of charge under license for use with the RC32614.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube and Instagram.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on